<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: When the STM/PIT module of MPC5775E is in freeze mode, will the timer still run in debug mode? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/When-the-STM-PIT-module-of-MPC5775E-is-in-freeze-mode-will-the/m-p/1369763#M19579</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1636617145566.png" style="width: 737px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/161916iB056956A2A228716/image-dimensions/737x130?v=v2" width="737" height="130" role="button" title="petervlna_0-1636617145566.png" alt="petervlna_0-1636617145566.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The counters are freeze in case you are in debug mode. Once you execute for example step in debug your core is executing instruction the counter will run and stop on next instruction halt. The counter will increment as it would during the instruction execution in real time. So you can see its proper value on next instruction.&lt;/P&gt;
&lt;P&gt;So you can see in debug mode how your counters increment. If you require the counter to be off in debug mode then simply disable them in debugger via script or via direct write to register.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Nov 2021 07:56:34 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2021-11-11T07:56:34Z</dc:date>
    <item>
      <title>When the STM/PIT module of MPC5775E is in freeze mode, will the timer still run in debug mode?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/When-the-STM-PIT-module-of-MPC5775E-is-in-freeze-mode-will-the/m-p/1369601#M19574</link>
      <description>&lt;P&gt;The freeze mode of the PIT timer in MPC5775ERM is described, but in my impression, the PIT is set to freeze mode. During online debugging, the timer will count. Is there a difference between the freeze mode between PIT and STM? In other words, after these two are set to freeze, they will not run during online debugging, or will the operation be suspended only when the online debugging is paused or interrupted?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 03:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/When-the-STM-PIT-module-of-MPC5775E-is-in-freeze-mode-will-the/m-p/1369601#M19574</guid>
      <dc:creator>yangmingsong</dc:creator>
      <dc:date>2021-11-11T03:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: When the STM/PIT module of MPC5775E is in freeze mode, will the timer still run in debug mode?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/When-the-STM-PIT-module-of-MPC5775E-is-in-freeze-mode-will-the/m-p/1369763#M19579</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1636617145566.png" style="width: 737px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/161916iB056956A2A228716/image-dimensions/737x130?v=v2" width="737" height="130" role="button" title="petervlna_0-1636617145566.png" alt="petervlna_0-1636617145566.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The counters are freeze in case you are in debug mode. Once you execute for example step in debug your core is executing instruction the counter will run and stop on next instruction halt. The counter will increment as it would during the instruction execution in real time. So you can see its proper value on next instruction.&lt;/P&gt;
&lt;P&gt;So you can see in debug mode how your counters increment. If you require the counter to be off in debug mode then simply disable them in debugger via script or via direct write to register.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 07:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/When-the-STM-PIT-module-of-MPC5775E-is-in-freeze-mode-will-the/m-p/1369763#M19579</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-11-11T07:56:34Z</dc:date>
    </item>
  </channel>
</rss>