<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC574xG other Derivatives debugging in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1362553#M19475</link>
    <description>&lt;P&gt;Please contact &lt;A href="mailto:support@lauterbach.com" target="_blank"&gt;support@lauterbach.com&lt;/A&gt;. In your email include a detailed description of the problem, including a screenshot of the error and the file resulting from menu Help -&amp;gt; Support -&amp;gt; System Information -&amp;gt; Save to File&lt;/P&gt;</description>
    <pubDate>Wed, 27 Oct 2021 15:43:52 GMT</pubDate>
    <dc:creator>rweiss</dc:creator>
    <dc:date>2021-10-27T15:43:52Z</dc:date>
    <item>
      <title>MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361284#M19458</link>
      <description>&lt;P&gt;Hello Dears,&lt;/P&gt;&lt;P&gt;I am going to use The Lauterbach trace32 debugger to work on&amp;nbsp; "MPC5746B". I am using the MPC574xG NXP sample application with the "run.cmm" file in it. I changed the derivative from MPC5746C to MPC5746B in the MCU module in EB. Then generate and compile without any errors. But Debugger was unable to program the flash of the chip. what is the problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ehsan&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 05:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361284#M19458</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-10-26T05:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361526#M19462</link>
      <description>&lt;P&gt;First please try to program FLASH using the original flash script ~~\demo\powerpc\flash\mpc574xg.cmm&lt;/P&gt;&lt;P&gt;If the problem remains, please explain in more detail.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Reinhard&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 09:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361526#M19462</guid>
      <dc:creator>rweiss</dc:creator>
      <dc:date>2021-10-26T09:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361602#M19463</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/18051"&gt;@rweiss&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Ok. I tried MPC574xG.cmm in demos... but it doesn't work. By the way I am able to program and flash this hardware with PE-Micro Multilink. In addition, I already have program and debug MPC574xP with Lauterbach trace32 using the same setup.&lt;BR /&gt;What should I do?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ehsan&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 10:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1361602#M19463</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-10-26T10:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1362553#M19475</link>
      <description>&lt;P&gt;Please contact &lt;A href="mailto:support@lauterbach.com" target="_blank"&gt;support@lauterbach.com&lt;/A&gt;. In your email include a detailed description of the problem, including a screenshot of the error and the file resulting from menu Help -&amp;gt; Support -&amp;gt; System Information -&amp;gt; Save to File&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 15:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1362553#M19475</guid>
      <dc:creator>rweiss</dc:creator>
      <dc:date>2021-10-27T15:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1364180#M19491</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/18051"&gt;@rweiss&lt;/a&gt;&amp;nbsp;I retry my works. And now the demo cmm file is running succrsfuly on the hardware. But its not working with run.cmm in the NXP mpc574xB-C-G sample folder. Where could I make change to solve this issue?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ehsan&lt;/P&gt;</description>
      <pubDate>Sun, 31 Oct 2021 19:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1364180#M19491</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-10-31T19:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC574xG other Derivatives debugging</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1364376#M19494</link>
      <description>&lt;P&gt;This is the error screenshot:&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 07:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC574xG-other-Derivatives-debugging/m-p/1364376#M19494</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-11-01T07:15:12Z</dc:date>
    </item>
  </channel>
</rss>