<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5777C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1357874#M19403</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I did some changes so project can be compiled and goes to you&amp;nbsp;int_dec_isr interrupt.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Tue, 19 Oct 2021 11:55:22 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-10-19T11:55:22Z</dc:date>
    <item>
      <title>MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1356433#M19371</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,The chip I use is mpc5777C, the IDE is S32DS2.1, and the program is added in the attachment. When I debug the Decrementer interrupt (interrupt number 10), the program will run away.&lt;BR /&gt;Proceed as follows:&lt;BR /&gt;First initialize the HID0 register, TSR, TCR register;&lt;BR /&gt;Then initialize IVPR and IVOR10;&lt;BR /&gt;Finally, the program will jump to IVOR10_Handler;&lt;BR /&gt;Please help me solve how the program jumps to interrupt No. 10 and executes related functions.&lt;/P&gt;&lt;P&gt;Respect&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 10:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1356433#M19371</guid>
      <dc:creator>PENGHAN</dc:creator>
      <dc:date>2021-10-15T10:54:20Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1357874#M19403</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I did some changes so project can be compiled and goes to you&amp;nbsp;int_dec_isr interrupt.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 19 Oct 2021 11:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1357874#M19403</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-10-19T11:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1643715#M23506</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I built the&amp;nbsp;MPC5777C_DSPI_Master_TXRX_DMA_S32DSPower21_Z7_0 project, I connected the SDO and SDI(loopback), I ran the code to see the&amp;nbsp;&amp;nbsp;DSPI_Master_Receive_Data is not udpated it always 0 any idea?, i can see the sck and SDO dataout on the scope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Mohamed.&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 15:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C/m-p/1643715#M23506</guid>
      <dc:creator>kaffel</dc:creator>
      <dc:date>2023-05-03T15:37:07Z</dc:date>
    </item>
  </channel>
</rss>