<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Signal ATRIG of eQADC is barely documented. Where to find the signal routing? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1356741#M19383</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;I'm currently making an I/O driver for the eQADC of the MPC5775B/E and I&lt;BR /&gt;want to make use of the streaming mode with CFIFO0. The documentation&lt;BR /&gt;(Reference Manual MPC5775E, Rev. 1, 05/2018, section 29) explains the need&lt;BR /&gt;of an Advance Trigger to start the streaming loop controlled by the normal&lt;BR /&gt;trigger (ETRIG). The entire section doesn't tell anything about where the&lt;BR /&gt;two trigger signals come from.&lt;/P&gt;&lt;P&gt;Ibid, sections 8.2.18f, SIU_ISEL4/5, describe multiplexers for choosing a&lt;BR /&gt;trigger signal for the command FIFOs but it looks much as if this relates&lt;BR /&gt;only to the normal trigger input ETRIG.&lt;/P&gt;&lt;P&gt;The entire reference manual (including Excel I/O attachment) has no&lt;BR /&gt;matches for "atrig" or "atrig0" outside of section 29, so I'm stuck.&lt;/P&gt;&lt;P&gt;Where do I find the information how to select an appropriate ATRIG signal?&lt;/P&gt;&lt;P&gt;How can I otherwise start the streaming mode?&lt;/P&gt;&lt;P&gt;The eQADC samples I found at&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777C" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777C&lt;/A&gt;&lt;BR /&gt;seem to all use the simple software trigger only. Is there a sample for&lt;BR /&gt;the streaming mode, too?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Peter&lt;/P&gt;</description>
    <pubDate>Sun, 17 Oct 2021 15:00:30 GMT</pubDate>
    <dc:creator>peter_vranken</dc:creator>
    <dc:date>2021-10-17T15:00:30Z</dc:date>
    <item>
      <title>Signal ATRIG of eQADC is barely documented. Where to find the signal routing?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1356741#M19383</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;I'm currently making an I/O driver for the eQADC of the MPC5775B/E and I&lt;BR /&gt;want to make use of the streaming mode with CFIFO0. The documentation&lt;BR /&gt;(Reference Manual MPC5775E, Rev. 1, 05/2018, section 29) explains the need&lt;BR /&gt;of an Advance Trigger to start the streaming loop controlled by the normal&lt;BR /&gt;trigger (ETRIG). The entire section doesn't tell anything about where the&lt;BR /&gt;two trigger signals come from.&lt;/P&gt;&lt;P&gt;Ibid, sections 8.2.18f, SIU_ISEL4/5, describe multiplexers for choosing a&lt;BR /&gt;trigger signal for the command FIFOs but it looks much as if this relates&lt;BR /&gt;only to the normal trigger input ETRIG.&lt;/P&gt;&lt;P&gt;The entire reference manual (including Excel I/O attachment) has no&lt;BR /&gt;matches for "atrig" or "atrig0" outside of section 29, so I'm stuck.&lt;/P&gt;&lt;P&gt;Where do I find the information how to select an appropriate ATRIG signal?&lt;/P&gt;&lt;P&gt;How can I otherwise start the streaming mode?&lt;/P&gt;&lt;P&gt;The eQADC samples I found at&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777C" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5777C&lt;/A&gt;&lt;BR /&gt;seem to all use the simple software trigger only. Is there a sample for&lt;BR /&gt;the streaming mode, too?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Peter&lt;/P&gt;</description>
      <pubDate>Sun, 17 Oct 2021 15:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1356741#M19383</guid>
      <dc:creator>peter_vranken</dc:creator>
      <dc:date>2021-10-17T15:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: Signal ATRIG of eQADC is barely documented. Where to find the signal routing?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1357195#M19391</link>
      <description>&lt;P&gt;SIU_ISEL4-7 chooses normal trigger (ETRIG) but this is also repeat trigger in streaming mode.&lt;/P&gt;
&lt;P&gt;SIU_ISEL9 selects Advance Trigger Source - this is basically ATRIG signal. As external signal ATRIG is not present with this device.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 12:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1357195#M19391</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-10-18T12:28:20Z</dc:date>
    </item>
    <item>
      <title>Re: Signal ATRIG of eQADC is barely documented. Where to find the signal routing?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1363336#M19484</link>
      <description>&lt;P&gt;Thanks a lot, got it. Driver is running well meanwhile&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 13:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Signal-ATRIG-of-eQADC-is-barely-documented-Where-to-find-the/m-p/1363336#M19484</guid>
      <dc:creator>peter_vranken</dc:creator>
      <dc:date>2021-10-28T13:53:35Z</dc:date>
    </item>
  </channel>
</rss>