<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Need TRK-MPC5604B CAN interface help</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257806#M193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved it: J1 needed to be connected 5-6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2013 08:52:44 GMT</pubDate>
    <dc:creator>jkm89</dc:creator>
    <dc:date>2013-05-28T08:52:44Z</dc:date>
    <item>
      <title>Need TRK-MPC5604B CAN interface help</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257803#M190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which jumpers must be connected to activate the SBC? Do I need external power?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 09:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257803#M190</guid>
      <dc:creator>jkm89</dc:creator>
      <dc:date>2013-05-27T09:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: Need TRK-MPC5604B CAN interface help</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257804#M191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm struggling myself with the CAN on a TRK-MPC5634 board. What I figured out so far, is that I need an external power supply (9-12V) and that the MC33903 needs to be set in DBG mode with a jumper (J5). Still I get nothing on the DB9 (CAN-H and CAN-L remain to 0V)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 10:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257804#M191</guid>
      <dc:creator>olivierkieffer</dc:creator>
      <dc:date>2013-05-27T10:57:49Z</dc:date>
    </item>
    <item>
      <title>Re: Need TRK-MPC5604B CAN interface help</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257805#M192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I emailed tech support about this issue and they said J5 needs to be installed and J4 needs to be removed (debug mode). Also, whenever I set the switch to the "on" position, the SBC starts getting very hot, which is concerning me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 01:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257805#M192</guid>
      <dc:creator>jkm89</dc:creator>
      <dc:date>2013-05-28T01:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: Need TRK-MPC5604B CAN interface help</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257806#M193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved it: J1 needed to be connected 5-6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 08:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257806#M193</guid>
      <dc:creator>jkm89</dc:creator>
      <dc:date>2013-05-28T08:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: Need TRK-MPC5604B CAN interface help</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257807#M194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And the CAN is working now? How do you check it?&lt;/P&gt;&lt;P&gt;I've attached a PEAK-USB interface and I always get a BUSHEAVY message ...&lt;/P&gt;&lt;P&gt;THE EVB is clearly terminated and I've put a 120Ohm resistor on the PEAK side. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 09:06:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Need-TRK-MPC5604B-CAN-interface-help/m-p/257807#M194</guid>
      <dc:creator>olivierkieffer</dc:creator>
      <dc:date>2013-05-28T09:06:18Z</dc:date>
    </item>
  </channel>
</rss>