<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Compile problem in MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1350990#M19299</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/111082"&gt;@hungnguyenphi&lt;/a&gt;, OK I cleared those expressions in vector_vle_mcal.s file, there wasn't any error in compile process, but the code didn't work correctly in debugging (trace32). Isn't it necessary to add or replace&amp;nbsp;Adc_Adcdig_EndGroupConvUnit0&amp;nbsp; with&amp;nbsp;Adc_Adcdig_EndGroupConvUnit1 for the proper performance of code? in debugging in the ADC task .c file it went on pending state and got stuck in timeout and breakout the code after.&lt;/P&gt;&lt;P&gt;I attached my startup file, kindly please find the attachment and take a look at it. thanks in advance...&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ehsan&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 06 Oct 2021 08:25:13 GMT</pubDate>
    <dc:creator>Ehsaaan</dc:creator>
    <dc:date>2021-10-06T08:25:13Z</dc:date>
    <item>
      <title>Compile problem in MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1349785#M19287</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;Dears&lt;/P&gt;&lt;P&gt;I have problems compiling this sample from NXP. According to the release note the project is configured and test for MPC5744P-144DC Adapter Board Rev C1 and etc... . I am going to run this sample on DEVKIT-MPC5744P from NXP(same chip and derivative). So I changed some configurations in EB Tresos on PORT, DIO, ADC, and PWM modules and changed the corresponding parameters according to this evaluation board. EB generation was ok but when I compiled the project using launch.bat, there were some errors in the generation. I attached the project files and some images from the configuration. thanks in advance for your help...&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ehsan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 03 Oct 2021 14:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1349785#M19287</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-10-03T14:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: Compile problem in MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1350344#M19291</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187713"&gt;@Ehsaaan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;As I can see, you are using&amp;nbsp; ADC1 instead ADC0, that why the&amp;nbsp;Adc_Adcdig_EndGroupConvUnit0 will not be defined and it should be removed in the Vector_vle_mcal.s file&lt;/P&gt;
&lt;P&gt;The same problem with the&amp;nbsp;FLEXPWM_0_SUBMOD_0_CMP_ISR. The&amp;nbsp;&lt;SPAN&gt;FLEXPWM_0_SUBMOD_0_CMP_ISR&lt;/SPAN&gt; is not defined in the Pwm_Cfg.h, because the PWM notification has been disabled in the GUI configuration. Then it should be removed in the Vector_vle_mcal.s file&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Hung&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 03:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1350344#M19291</guid>
      <dc:creator>hungnguyenphi</dc:creator>
      <dc:date>2021-10-05T03:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: Compile problem in MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1350990#M19299</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/111082"&gt;@hungnguyenphi&lt;/a&gt;, OK I cleared those expressions in vector_vle_mcal.s file, there wasn't any error in compile process, but the code didn't work correctly in debugging (trace32). Isn't it necessary to add or replace&amp;nbsp;Adc_Adcdig_EndGroupConvUnit0&amp;nbsp; with&amp;nbsp;Adc_Adcdig_EndGroupConvUnit1 for the proper performance of code? in debugging in the ADC task .c file it went on pending state and got stuck in timeout and breakout the code after.&lt;/P&gt;&lt;P&gt;I attached my startup file, kindly please find the attachment and take a look at it. thanks in advance...&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ehsan&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 08:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1350990#M19299</guid>
      <dc:creator>Ehsaaan</dc:creator>
      <dc:date>2021-10-06T08:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: Compile problem in MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1352196#M19310</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187713"&gt;@Ehsaaan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The vle file is correct, but please also update the file&amp;nbsp;sample_app_mcal_initialization_task.c. We should enable the interrupt number 500 but not 496(because currently we use ADC1 but not ADC0).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hungnguyenphi_0-1633654690028.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158549iD068DA8AA7C32E60/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hungnguyenphi_0-1633654690028.png" alt="hungnguyenphi_0-1633654690028.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Hung&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 00:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Compile-problem-in-MPC574XP-MCAL4-0-RTM-2-0-2-Sample-Application/m-p/1352196#M19310</guid>
      <dc:creator>hungnguyenphi</dc:creator>
      <dc:date>2021-10-08T00:58:40Z</dc:date>
    </item>
  </channel>
</rss>