<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Read-While-Write on MPC5675K Code Flash modules</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1349439#M19285</link>
    <description>&lt;P&gt;David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your answer!&lt;/P&gt;&lt;P&gt;It explains a lot.&lt;/P&gt;&lt;P&gt;Thank you also for your little example on Data Flash use &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Oct 2021 05:44:15 GMT</pubDate>
    <dc:creator>JChMathae</dc:creator>
    <dc:date>2021-10-01T05:44:15Z</dc:date>
    <item>
      <title>Read-While-Write on MPC5675K Code Flash modules</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1347306#M19264</link>
      <description>&lt;LI-SPOILER&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;According to the MPC5675K Reference Manual in chapter 8 "Flash Memory", Read-While-Write accesses within a Flash module is not possible. That is, it is impossible to erase or program a Flash sector when executing code from another sector within the same Flash module.&lt;BR /&gt;&lt;BR /&gt;But when I am using the Standard Software C90LC Driver it seems to do exactly that: executing from a Flash module sector when erasing/programming another sector within this same Flash module...&lt;BR /&gt;&lt;BR /&gt;Where is the truth?!&lt;BR /&gt;&lt;BR /&gt;Thank you for your help.&lt;BR /&gt;&lt;BR /&gt;Best regards.&lt;/LI-SPOILER&gt;</description>
      <pubDate>Tue, 28 Sep 2021 06:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1347306#M19264</guid>
      <dc:creator>JChMathae</dc:creator>
      <dc:date>2021-09-28T06:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: Read-While-Write on MPC5675K Code Flash modules</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1348236#M19275</link>
      <description>&lt;P&gt;Hi, by default bus stall happens instead of RWW, thus example will run even without relocation to SRAM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1632906282423.png" style="width: 644px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/157874i94C3D395477EC6C6/image-dimensions/644x536?v=v2" width="644" height="536" role="button" title="davidtosenovjan_0-1632906282423.png" alt="davidtosenovjan_0-1632906282423.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;However driver also includes macro COPY_TO_RAM, so you can simply relocate flash routine to the SRAM, what you should do in real application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 09:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1348236#M19275</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-09-29T09:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: Read-While-Write on MPC5675K Code Flash modules</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1349439#M19285</link>
      <description>&lt;P&gt;David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your answer!&lt;/P&gt;&lt;P&gt;It explains a lot.&lt;/P&gt;&lt;P&gt;Thank you also for your little example on Data Flash use &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 05:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-While-Write-on-MPC5675K-Code-Flash-modules/m-p/1349439#M19285</guid>
      <dc:creator>JChMathae</dc:creator>
      <dc:date>2021-10-01T05:44:15Z</dc:date>
    </item>
  </channel>
</rss>