<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EQADC Streaming Mode on MPC5777C in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EQADC-Streaming-Mode-on-MPC5777C/m-p/1343068#M19196</link>
    <description>&lt;P&gt;Hi, yes, you can do it. It should be no issue.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Sep 2021 06:31:22 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2021-09-21T06:31:22Z</dc:date>
    <item>
      <title>EQADC Streaming Mode on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-Streaming-Mode-on-MPC5777C/m-p/1342775#M19194</link>
      <description>&lt;P&gt;I would like to ask a question about EQADC Streaming mode on MPC5777C.&lt;/P&gt;&lt;P&gt;My purpose is to read just one data from EQADC with each hardware trigger. Hence, I am writing one command on CFIFO and also I am setting repeat and pause bit on same command in order to run streaming mode. I did not encounter any warning or note about that on reference manuel. Can I set both REP and STOP bit on same conversion command?&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;&lt;P&gt;Berat.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 13:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-Streaming-Mode-on-MPC5777C/m-p/1342775#M19194</guid>
      <dc:creator>berat24</dc:creator>
      <dc:date>2021-09-20T13:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: EQADC Streaming Mode on MPC5777C</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EQADC-Streaming-Mode-on-MPC5777C/m-p/1343068#M19196</link>
      <description>&lt;P&gt;Hi, yes, you can do it. It should be no issue.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Sep 2021 06:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EQADC-Streaming-Mode-on-MPC5777C/m-p/1343068#M19196</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-09-21T06:31:22Z</dc:date>
    </item>
  </channel>
</rss>