<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FlexRay CycleCounter Init value at MPC5674F in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1316125#M18792</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;per my understanding,&lt;BR /&gt;1. yes&lt;BR /&gt;2. communication will not work&lt;BR /&gt;3. in cycle 10&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jul 2021 19:44:25 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-07-30T19:44:25Z</dc:date>
    <item>
      <title>FlexRay CycleCounter Init value at MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1313853#M18747</link>
      <description>&lt;P&gt;Hi, I m using MPC5674F for Flexray application.&lt;/P&gt;&lt;P&gt;I want to know the cycle counter when the core starts Flexray communication after being normal active.&lt;/P&gt;&lt;P&gt;I expected that cycle counter is 0 for all nodes within flexray network. But it was not 0 and different.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 11:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1313853#M18747</guid>
      <dc:creator>cjw-442</dc:creator>
      <dc:date>2021-07-27T11:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRay CycleCounter Init value at MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1315144#M18777</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, it could be nonzero as bus setup must be done before node switch to normal active, as shown in Fig. 37 of AN12233;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12233.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12233.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 08:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1315144#M18777</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-07-29T08:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRay CycleCounter Init value at MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1315539#M18787</link>
      <description>&lt;P&gt;Thank you for quick Reply, Petr.&lt;/P&gt;&lt;P&gt;Our Flexray Parameters are as follows.&lt;/P&gt;&lt;P&gt;&amp;nbsp; - Communication Cycle is 500 us / 5 ms.&lt;/P&gt;&lt;P&gt;&amp;nbsp; - 2 Nodes are in Flexray Cluster (3 nodes will be joined later)&lt;/P&gt;&lt;P&gt;&amp;nbsp; - 3 Static slots (Using Key slot) / Only Dynamic Slots are using for Data Exchange.&lt;/P&gt;&lt;P&gt;I have three questions here.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 1.&amp;nbsp;Do all nodes coupled to Flexray communication use the same Cycle Counter?&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. If 1 is correct, how will Flexray communication be affected if the Cycle Counter between nodes is different?&lt;/P&gt;&lt;P&gt;&amp;nbsp; 3.&amp;nbsp;When node 1 sends data to Cycle 10, Slot 1, when does node 2 actually receive data?&lt;BR /&gt;Is it Cycle 10 or 11?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 02:05:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1315539#M18787</guid>
      <dc:creator>cjw-442</dc:creator>
      <dc:date>2021-07-30T02:05:44Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRay CycleCounter Init value at MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1316125#M18792</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;per my understanding,&lt;BR /&gt;1. yes&lt;BR /&gt;2. communication will not work&lt;BR /&gt;3. in cycle 10&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jul 2021 19:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1316125#M18792</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-07-30T19:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRay CycleCounter Init value at MPC5674F</title>
      <link>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1461181#M21208</link>
      <description>&lt;P&gt;I also set the cycle counter filter related registers. But it seems not work. At non-assigned cycle, the frame transmit as a null frame. Do you have this problems?(I use MPC5748G)&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 01:28:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/FlexRay-CycleCounter-Init-value-at-MPC5674F/m-p/1461181#M21208</guid>
      <dc:creator>Lyn</dc:creator>
      <dc:date>2022-05-20T01:28:58Z</dc:date>
    </item>
  </channel>
</rss>