<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Display configuration in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1308965#M18686</link>
    <description>&lt;P&gt;Hi, do you have correctly connected RGB signals according panel manufacturer's datasheet?&lt;/P&gt;
&lt;P&gt;Have you checked AN4187?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4187.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4187.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Jul 2021 08:28:43 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2021-07-16T08:28:43Z</dc:date>
    <item>
      <title>Display configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1307831#M18678</link>
      <description>&lt;P&gt;Hi Nxp team,&lt;/P&gt;&lt;P&gt;We are working on xpc560s EVB (176 pin module) for developing low-cost instrument cluster.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We used New Heaven display (&amp;nbsp;&lt;SPAN&gt;NHD&lt;/SPAN&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;SPAN&gt;4.3&lt;/SPAN&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;SPAN&gt;800480C&lt;/SPAN&gt;&lt;SPAN&gt;F&lt;/SPAN&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;SPAN&gt;AS&lt;/SPAN&gt;&lt;SPAN&gt;XP&lt;/SPAN&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;SPAN&gt;CTP) with lab0 code for this exercise.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We first tried to test the interface between DCU and the TFT LCD panel by using color bar mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We could mode two observations from this,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. When the&amp;nbsp; Invert Horizontal &amp;amp; Vertical Synchronize signals (from SYN_POL Register) is active low we can see the pattern but the color is not matching(attached the image below-colour_bar_H_V_Inv.jpg) as per the COL_BAR1..8 Register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.When the&amp;nbsp;Invert Horizontal &amp;amp; Vertical Synchronize signals (from SYN_POL Register) is active high we can see some pattern as per the COL_BAR1..8 Register(Image-colour_bar_H_V.jpg) but some are missing in the sequence.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;DCU is configured as per the&amp;nbsp;New Heaven display (&amp;nbsp;NHD-4.3-800480CF-ASXP-CTP).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;RASTER_EN bit was also enabled in this exercise.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Kindly verify which observation is correct and guide us to proceed further.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Vivishekh&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 16:22:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1307831#M18678</guid>
      <dc:creator>tech_mofu</dc:creator>
      <dc:date>2021-07-14T16:22:26Z</dc:date>
    </item>
    <item>
      <title>Re: Display configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1308965#M18686</link>
      <description>&lt;P&gt;Hi, do you have correctly connected RGB signals according panel manufacturer's datasheet?&lt;/P&gt;
&lt;P&gt;Have you checked AN4187?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4187.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4187.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 08:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1308965#M18686</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-07-16T08:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Display configuration</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1309765#M18704</link>
      <description>&lt;P&gt;Thanks David for the inputs.&lt;/P&gt;&lt;P&gt;We did not configure the DE (Display enable) port correctly. Once we configured appropriately at the DCU side it worked.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tested the Bar graphs and Freescale bitmap display and it worked.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Raghu&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 10:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Display-configuration/m-p/1309765#M18704</guid>
      <dc:creator>tech_mofu</dc:creator>
      <dc:date>2021-07-19T10:23:28Z</dc:date>
    </item>
  </channel>
</rss>