<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5748G-FREERTOS_code migrate</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1307454#M18673</link>
    <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i tried&amp;nbsp; with this code using uart data, i am not using any external hardware now(like gsm) , i send the data through hyperterminal uart&amp;nbsp; here transmitter&amp;nbsp; working but i can,t get the output when i receive data from hyperterminal .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uart is working both tx/rx alone .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;kalai&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jul 2021 07:08:52 GMT</pubDate>
    <dc:creator>kalai</dc:creator>
    <dc:date>2021-07-14T07:08:52Z</dc:date>
    <item>
      <title>MPC5748G-FREERTOS_code migrate</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1303663#M18603</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;i migrate the code one controller (s32k148 ) to another controller MPc5748G ,i get the output from transmitter section but i cant receive the data i dont know what is issue.so please refer&amp;nbsp; the code and suggest me the solution&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i will attach the code below .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 06:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1303663#M18603</guid>
      <dc:creator>kalai</dc:creator>
      <dc:date>2021-07-07T06:40:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G-FREERTOS_code migrate</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1306724#M18665</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Hmm, its hard to say.&lt;/P&gt;
&lt;P&gt;I can only guess, did you initialized peripherals properly (like SIUL unit for pins assignment) ?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jul 2021 08:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1306724#M18665</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-07-13T08:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G-FREERTOS_code migrate</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1307454#M18673</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i tried&amp;nbsp; with this code using uart data, i am not using any external hardware now(like gsm) , i send the data through hyperterminal uart&amp;nbsp; here transmitter&amp;nbsp; working but i can,t get the output when i receive data from hyperterminal .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uart is working both tx/rx alone .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;kalai&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 07:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-FREERTOS-code-migrate/m-p/1307454#M18673</guid>
      <dc:creator>kalai</dc:creator>
      <dc:date>2021-07-14T07:08:52Z</dc:date>
    </item>
  </channel>
</rss>