<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: about FlexPWM</title>
    <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467407#M1853</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #2873ee;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;The OUT23 and OUT45 are implemented to device so user can select the level of signal during deadtime.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;OUT23 bit is only used when SEL23 for submodule 0 is set to 0b10.&amp;nbsp; It allows software control of which signal is supplied to the deadtime generator of that submodule.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;1 = A logic 1 is supplied to the deadtime generator of submodule 0 instead of PWM23 or PWM45.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;0 = A logic 0 is supplied to the deadtime generator of submodule 0 instead of PWM23 or PWM45.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;The SEL23 and SEL45 fields each choose from one of four signals that can be supplied to the submodule outputs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;So if your SEL23 is configured for OUT23 then on the module output you will see the signal according to SWCOUT register configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22106iB63EA1050F463446/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jan 2016 12:03:32 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2016-01-27T12:03:32Z</dc:date>
    <item>
      <title>about FlexPWM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467406#M1852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi. I'm studying FlexPWM about MPC5643L. &lt;/P&gt;&lt;P&gt;I can't understand OUT23 and PWM23. In reference manual, I can select that using Deadtime Source Select Register(DTSRCSEL).&lt;/P&gt;&lt;P&gt;I understand that PWM23 is generated from comparing counter register(CNT) and value register(VAL2, VAL3).&lt;/P&gt;&lt;P&gt;But i can't find how OUT23 is generated.&lt;/P&gt;&lt;P&gt;And i don't understand deadtime logic.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you explain this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Juhyung&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 08:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467406#M1852</guid>
      <dc:creator>motman</dc:creator>
      <dc:date>2016-01-27T08:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: about FlexPWM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467407#M1853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #2873ee;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;The OUT23 and OUT45 are implemented to device so user can select the level of signal during deadtime.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;OUT23 bit is only used when SEL23 for submodule 0 is set to 0b10.&amp;nbsp; It allows software control of which signal is supplied to the deadtime generator of that submodule.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;1 = A logic 1 is supplied to the deadtime generator of submodule 0 instead of PWM23 or PWM45.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;0 = A logic 0 is supplied to the deadtime generator of submodule 0 instead of PWM23 or PWM45.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;The SEL23 and SEL45 fields each choose from one of four signals that can be supplied to the submodule outputs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0070c0;"&gt;So if your SEL23 is configured for OUT23 then on the module output you will see the signal according to SWCOUT register configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22106iB63EA1050F463446/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 12:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467407#M1853</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-01-27T12:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: about FlexPWM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467408#M1854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Peter.&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;You mean that SWCOUT register select OUT23 or OUT45 value. Right?&lt;/P&gt;&lt;P&gt;SWCOUT register control output as Force out. I don't know what i think.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And, Can you have a PWM capture example? If you have, can you explain how can initialize, how can use. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Juhyung.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 04:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467408#M1854</guid>
      <dc:creator>motman</dc:creator>
      <dc:date>2016-01-29T04:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: about FlexPWM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467409#M1855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OUT23 -&amp;gt; PWMA of selected submodule - It allows software control of which signal is supplied to the deadtime generator of that submodule.&lt;/P&gt;&lt;P&gt;OUT45 -&amp;gt; PWMB of selected submodule - It allows software control of which signal is supplied to the deadtime generator of that submodule.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 11:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467409#M1855</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2016-02-01T11:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: about FlexPWM</title>
      <link>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467410#M1856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;refer to the attached example. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The Submodule0 is set to generate independent PWMA and PWMB signals. The PWMX is used as input for the Capture feature. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Capture logic is set to capture one rising and one falling edge in one shot mode. Thus you can check the edge placing and calculate a generated duty cycle.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 11:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/about-FlexPWM/m-p/467410#M1856</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-02-02T11:48:25Z</dc:date>
    </item>
  </channel>
</rss>