<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RappId Bootloader Utility in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1283869#M18366</link>
    <description>&lt;P&gt;Thanks for the reply Petr,&lt;/P&gt;&lt;P&gt;So, if wanted to erase only a particular section of flash starting from some random flash address, is this possible with RappiD.?&lt;/P&gt;&lt;P&gt;Because in the Rappid Release notes, it is written that both the options "Eras Flash Only" and "Erase &amp;amp; Program" will completely erase the flash area.&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 04:52:28 GMT</pubDate>
    <dc:creator>maharajshreekum</dc:creator>
    <dc:date>2021-05-28T04:52:28Z</dc:date>
    <item>
      <title>RappId Bootloader Utility</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1282606#M18344</link>
      <description>&lt;P&gt;I wanted to know while flashing the bootloader code and app image code to the MPC5748 Dev kit,&lt;/P&gt;&lt;P&gt;What is the purpose of selecting the Start Address when the Rappid tool itself clears all the flash?&lt;/P&gt;&lt;P&gt;How we will make sure that the bootloader code is not erased after flashing the application image, since both "Erash flash Only" &amp;amp;&amp;nbsp; "Erase and Program" option clears the entire flash.&lt;/P&gt;&lt;P&gt;Or I have misunderstood the concept of serial bootloader for MPC 5748G ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please help!!&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 14:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1282606#M18344</guid>
      <dc:creator>maharajshreekum</dc:creator>
      <dc:date>2021-05-26T14:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: RappId Bootloader Utility</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1283445#M18356</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;start address is the address Rappid bootloader jumps to after the application code is downloaded.&lt;BR /&gt;Rappid bootloader is located at flash block started at 0x78C000 and this block is locked by bootloader code, so will not be erased.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 11:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1283445#M18356</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-05-27T11:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: RappId Bootloader Utility</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1283869#M18366</link>
      <description>&lt;P&gt;Thanks for the reply Petr,&lt;/P&gt;&lt;P&gt;So, if wanted to erase only a particular section of flash starting from some random flash address, is this possible with RappiD.?&lt;/P&gt;&lt;P&gt;Because in the Rappid Release notes, it is written that both the options "Eras Flash Only" and "Erase &amp;amp; Program" will completely erase the flash area.&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 04:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1283869#M18366</guid>
      <dc:creator>maharajshreekum</dc:creator>
      <dc:date>2021-05-28T04:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: RappId Bootloader Utility</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1291192#M18465</link>
      <description>&lt;P&gt;no that is not possible with RAppID bootloader&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 07:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RappId-Bootloader-Utility/m-p/1291192#M18465</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-06-11T07:47:15Z</dc:date>
    </item>
  </channel>
</rss>