<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5606B startertrak board max input voltage for port pins in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280280#M18277</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.&lt;/P&gt;
&lt;P&gt;The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 21 May 2021 09:18:27 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-05-21T09:18:27Z</dc:date>
    <item>
      <title>MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1279829#M18268</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using mpc5606b startertrak dev board . I have attached external transceivers TJA1050 with the CAN bus pins. I have supplied 5V to transceivers and thus the same logic voltage is applied to CAN port pins of mpc5606b. Can mpc5606b pins take 5V input? Will it damage the pins?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 May 2021 14:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1279829#M18268</guid>
      <dc:creator>sundar19</dc:creator>
      <dc:date>2021-05-20T14:13:07Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280280#M18277</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.&lt;/P&gt;
&lt;P&gt;The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 09:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280280#M18277</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-05-21T09:18:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280364#M18282</link>
      <description>&lt;P&gt;Thank you so much&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 11:21:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280364#M18282</guid>
      <dc:creator>sundar19</dc:creator>
      <dc:date>2021-05-21T11:21:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280369#M18283</link>
      <description>&lt;P&gt;You saying that if I power up mpc5606b with 3.3V , then its pins arent 5V tolerant?&amp;nbsp;&lt;BR /&gt;thank you&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 11:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280369#M18283</guid>
      <dc:creator>sundar19</dc:creator>
      <dc:date>2021-05-21T11:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280373#M18284</link>
      <description>&lt;P&gt;Yes, you can find in the datasheet:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1621596721976.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145226i933DB5834AE4EEAA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1621596721976.png" alt="lukaszadrapa_0-1621596721976.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 11:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280373#M18284</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-05-21T11:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B startertrak board max input voltage for port pins</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280376#M18285</link>
      <description>&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 11:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-startertrak-board-max-input-voltage-for-port-pins/m-p/1280376#M18285</guid>
      <dc:creator>sundar19</dc:creator>
      <dc:date>2021-05-21T11:37:01Z</dc:date>
    </item>
  </channel>
</rss>