<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mpc5748g Bus Off register in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-Bus-Off-register/m-p/1262338#M17982</link>
    <description>&lt;P&gt;Hi, I got really helpful answer for my last question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-Bus-Off/m-p/1261695#M17968" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-Bus-Off/m-p/1261695#M17968&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a one more question.&lt;/P&gt;&lt;P&gt;CAN_ESR1.BOFFDONEINT is set after counting 128 occurrences of 11 consecutive recessive bits on the CAN bus.&lt;/P&gt;&lt;P&gt;And if CAN_ERS2.BOFFDONEMSK is set, an interrupt is generated to the CPU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How is this related with CAN_CTRL1.BOFFREC bit?&lt;/P&gt;&lt;P&gt;I asserted CAN_CTRL1.BOFFREC(disable auto recovery) and asserted CAN_ERS2.BOFFDONEMSK, but didn't get out of the Bus-off state.&lt;/P&gt;&lt;P&gt;Is CAN_CTRL1.BOFFREC bit only related to get out of the Bus-Off state?&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 22:54:36 GMT</pubDate>
    <dc:creator>skseofh</dc:creator>
    <dc:date>2021-04-14T22:54:36Z</dc:date>
    <item>
      <title>mpc5748g Bus Off register</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-Bus-Off-register/m-p/1262338#M17982</link>
      <description>&lt;P&gt;Hi, I got really helpful answer for my last question.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-Bus-Off/m-p/1261695#M17968" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-Bus-Off/m-p/1261695#M17968&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a one more question.&lt;/P&gt;&lt;P&gt;CAN_ESR1.BOFFDONEINT is set after counting 128 occurrences of 11 consecutive recessive bits on the CAN bus.&lt;/P&gt;&lt;P&gt;And if CAN_ERS2.BOFFDONEMSK is set, an interrupt is generated to the CPU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How is this related with CAN_CTRL1.BOFFREC bit?&lt;/P&gt;&lt;P&gt;I asserted CAN_CTRL1.BOFFREC(disable auto recovery) and asserted CAN_ERS2.BOFFDONEMSK, but didn't get out of the Bus-off state.&lt;/P&gt;&lt;P&gt;Is CAN_CTRL1.BOFFREC bit only related to get out of the Bus-Off state?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 22:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5748g-Bus-Off-register/m-p/1262338#M17982</guid>
      <dc:creator>skseofh</dc:creator>
      <dc:date>2021-04-14T22:54:36Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5748g Bus Off register</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-Bus-Off-register/m-p/1263037#M18000</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, in manual recover mode you have to clear&amp;nbsp;&lt;SPAN&gt;BOFFREC&amp;nbsp;so you can get out of bus off state. After leaving bus off you can set&amp;nbsp;BOFFREC&amp;nbsp;again.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 19:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5748g-Bus-Off-register/m-p/1263037#M18000</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-04-15T19:29:58Z</dc:date>
    </item>
  </channel>
</rss>