<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EEprom emulation driver for MPC5604B in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465787#M1793</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are two files common for all compilers:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Program Files (x86)\Freescale\EEE_Driver_v1.3.0\MPC5xxx\Demos\src\C90\C90LC_DF\MPC5604P\ intc_branch_table_vle.s&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;C:\Program Files (x86)\Freescale\EEE_Driver_v1.3.0\MPC5xxx\Demos\src\C90\IVOR2_vle.s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is necessary to change this line in both files from:&lt;/P&gt;&lt;P&gt;.equ COMPILER,&amp;nbsp;&amp;nbsp;&amp;nbsp; GHS&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;.equ COMPILER,&amp;nbsp;&amp;nbsp;&amp;nbsp; CW&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then it will work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn’t test it but I believe it will work also on MPC5604B. I can see in the source files that it doesn’t touch specific features but rather flash only, so it should work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 10:14:20 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2016-05-12T10:14:20Z</dc:date>
    <item>
      <title>EEprom emulation driver for MPC5604B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465786#M1792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We used MPC5604B to develop our project. In our planning, Internal data flash could be instead of&amp;nbsp;&amp;nbsp; EEprom. So we downloaded MPC5xxx_EEE_DRIVER.exe&amp;nbsp; from official website.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Then we tried to compile the demo project(in ..\Demos\build\MPC5604P_CW_VLE folder), two errors were displayed in message box as below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="149164_149164.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121587i1C33D7E5B3BE2B7E/image-size/large?v=v2&amp;amp;px=999" role="button" title="149164_149164.png" alt="149164_149164.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57096i996606D4DA6F7993/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The IDE can't recognize the .vle opcode. But VLE configuration were already be opened.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="149171_149171.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121588iF99FD61D9EDF3A19/image-size/large?v=v2&amp;amp;px=999" role="button" title="149171_149171.png" alt="149171_149171.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57129iCF5129A5198583BE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is there something wrong with the demo project? how to solve this problem?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we used the MPC5604P demo code as EEprom emulation driver for MPC5604B, does the ecu can operate normally?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 07:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465786#M1792</guid>
      <dc:creator>朱先生</dc:creator>
      <dc:date>2016-05-12T07:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: EEprom emulation driver for MPC5604B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465787#M1793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are two files common for all compilers:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Program Files (x86)\Freescale\EEE_Driver_v1.3.0\MPC5xxx\Demos\src\C90\C90LC_DF\MPC5604P\ intc_branch_table_vle.s&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;C:\Program Files (x86)\Freescale\EEE_Driver_v1.3.0\MPC5xxx\Demos\src\C90\IVOR2_vle.s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is necessary to change this line in both files from:&lt;/P&gt;&lt;P&gt;.equ COMPILER,&amp;nbsp;&amp;nbsp;&amp;nbsp; GHS&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;.equ COMPILER,&amp;nbsp;&amp;nbsp;&amp;nbsp; CW&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then it will work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn’t test it but I believe it will work also on MPC5604B. I can see in the source files that it doesn’t touch specific features but rather flash only, so it should work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 10:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465787#M1793</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-05-12T10:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: EEprom emulation driver for MPC5604B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465788#M1794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Lukas:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Our compiler is Codeworrior, not GreenHills. I forget to configure the compiler option in demo code. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I change the code according to your advise, the ecu can normally work. Thanks for your information, very useful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bryce.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 23:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465788#M1794</guid>
      <dc:creator>朱先生</dc:creator>
      <dc:date>2016-05-12T23:21:00Z</dc:date>
    </item>
    <item>
      <title>Re: EEprom emulation driver for MPC5604B</title>
      <link>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465789#M1795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Lukas:&lt;/P&gt;&lt;P&gt;   I change the code according to your advise, The build process has been done with no error. The ecu can normally work.&lt;/P&gt;&lt;P&gt;  Thanks for your reply. &lt;/P&gt;&lt;P&gt;  &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;   Regards,&lt;/P&gt;&lt;P&gt;   Bryce&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 23:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/EEprom-emulation-driver-for-MPC5604B/m-p/465789#M1795</guid>
      <dc:creator>朱先生</dc:creator>
      <dc:date>2016-05-12T23:21:47Z</dc:date>
    </item>
  </channel>
</rss>