<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 MPC5777C - Power up sequence</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1257190#M17895</link>
    <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;in AN5268 - MPC5777C Hardware Requirements_Example Circuits (Rev. 0.06 / 2016), Chapter 3.4, you write "Power up VDDPMC / VDDPWR, VDDA_MISC, VDDA_EQ, and all VDDEx / VDDEHx supplies first and then power up VDD."&lt;/P&gt;&lt;P&gt;We made an external power supply 1.25 V, 3.3 V and 5 V with a sequence that the 1.25 V (VDD) rises by 200 ms after a voltage of 3.3 V and 5 V. With such a sequence, the processor on the evolution board MPC5777C-DEVB_QSG (SCH-29962) did not start. By measuring, we found that the evolution board has power up of 1.25 V almost at the same with a voltage 3.3 V and 5 V. We then adjusted our external power supply so that all voltage sources power up at the same time and the processor started up.&lt;/P&gt;&lt;P&gt;Is there any limit (min., nom., max.) for the delay of the supply 1,25V power up &amp;nbsp;after 3.3V and 5V? In our experience, 200 ms is too much.&lt;/P&gt;</description>
    <pubDate>Tue, 06 Apr 2021 09:18:00 GMT</pubDate>
    <dc:creator>kardos_michal</dc:creator>
    <dc:date>2021-04-06T09:18:00Z</dc:date>
    <item>
      <title>MPC5777C - Power up sequence</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1257190#M17895</link>
      <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;in AN5268 - MPC5777C Hardware Requirements_Example Circuits (Rev. 0.06 / 2016), Chapter 3.4, you write "Power up VDDPMC / VDDPWR, VDDA_MISC, VDDA_EQ, and all VDDEx / VDDEHx supplies first and then power up VDD."&lt;/P&gt;&lt;P&gt;We made an external power supply 1.25 V, 3.3 V and 5 V with a sequence that the 1.25 V (VDD) rises by 200 ms after a voltage of 3.3 V and 5 V. With such a sequence, the processor on the evolution board MPC5777C-DEVB_QSG (SCH-29962) did not start. By measuring, we found that the evolution board has power up of 1.25 V almost at the same with a voltage 3.3 V and 5 V. We then adjusted our external power supply so that all voltage sources power up at the same time and the processor started up.&lt;/P&gt;&lt;P&gt;Is there any limit (min., nom., max.) for the delay of the supply 1,25V power up &amp;nbsp;after 3.3V and 5V? In our experience, 200 ms is too much.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 09:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1257190#M17895</guid>
      <dc:creator>kardos_michal</dc:creator>
      <dc:date>2021-04-06T09:18:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C - Power up sequence</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1257813#M17903</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;evolution board MPC5777C-DEVB_QSG (SCH-29962)&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Do you mean NXP evaluation board?&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;We made an external power supply 1.25 V, 3.3 V and 5 V with a sequence that the 1.25 V (VDD) rises by 200 ms after a voltage of 3.3 V and 5 V&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;The micro will be held in reset until the core voltage rise to 1.2V. No execution is performed.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;By measuring, we found that the evolution board has power up of 1.25 V almost at the same with a voltage 3.3 V and 5 V.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Yes, as this is most common case when you want to start your application as soon as possible after power is applied.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is there any limit (min., nom., max.) for the delay of the supply 1,25V power up after 3.3V and 5V? In our experience, 200 ms is too much.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No, there is no limit defined for that. Usually you want to have micro fully operational in less then 100ms.&lt;/P&gt;
&lt;P&gt;power up sequence with all tests could take 20-40ms + startup code another 50ms. So you apply the core voltage in same time as VDD_HV or if its generated from HV, then there a slight delay.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 08:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1257813#M17903</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-04-07T08:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777C - Power up sequence</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1261755#M17971</link>
      <description>&lt;P&gt;Hello Peter,&lt;BR /&gt;Thank you for your response. I have no further questions about that.&lt;/P&gt;&lt;P&gt;Yes, it was meant NXP evolution board.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 07:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777C-Power-up-sequence/m-p/1261755#M17971</guid>
      <dc:creator>kardos_michal</dc:creator>
      <dc:date>2021-04-14T07:05:06Z</dc:date>
    </item>
  </channel>
</rss>