<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to import NXP Autosar MCAL Sample Application in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1254763#M17876</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If I understand correctly your question, then we don't provide the RTE and OS stack, so it's pretty much depended on the 3rd party who provides these package to make their RTE and OS stack to compatible with EB Tresos 14.2.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Nam&lt;/P&gt;</description>
    <pubDate>Wed, 31 Mar 2021 07:11:06 GMT</pubDate>
    <dc:creator>namnguyenviet</dc:creator>
    <dc:date>2021-03-31T07:11:06Z</dc:date>
    <item>
      <title>Unable to import NXP Autosar MCAL Sample Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1253780#M17862</link>
      <description>&lt;P&gt;Hi Team&lt;BR /&gt;&lt;BR /&gt;I managed to install MCAL and Tresos.&lt;BR /&gt;Now i am trying to import the MCAL Sample Application. During the import i 1st hit the error related to updating 103 to 105. I did that in all xdm project inside tresos/workspace/.pref&lt;BR /&gt;But now after that i am hitting the error as shown below.&lt;BR /&gt;Do i need to further update the Sample MCAL application to work on MCAL 1.0.5 ?&lt;BR /&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error_samplemcal_application.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140890i427217EB1F2CBC4B/image-size/large?v=v2&amp;amp;px=999" role="button" title="error_samplemcal_application.PNG" alt="error_samplemcal_application.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any support to resolve this would be highly appreciated.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Malai&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 19:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1253780#M17862</guid>
      <dc:creator>cmalai</dc:creator>
      <dc:date>2021-03-29T19:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to import NXP Autosar MCAL Sample Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1253959#M17863</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which project you're trying to import? Is that the sample from MPC574xG ASR 4.0 RTM 1.0.5 or RTM 1.0.3?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Anyway, the error log says that you're missing the OS package, which is a separate one rather than included in the MCAL package. You can find it here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/mpc5xxx-microcontrollers/ultra-reliable-mpc57xx-mcus/ultra-reliable-mcus-for-automotive-and-industrial-control-and-gateway:MPC574xB-C-G?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/mpc5xxx-microcontrollers/ultra-reliable-mpc57xx-mcus/ultra-reliable-mcus-for-automotive-and-industrial-control-and-gateway:MPC574xB-C-G?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="namnguyenviet_0-1617076816169.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140922i149D80F6D07B3AE2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="namnguyenviet_0-1617076816169.png" alt="namnguyenviet_0-1617076816169.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can consider not using OS. In this case, just click to the Remove module button to remove it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 04:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1253959#M17863</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2021-03-30T04:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to import NXP Autosar MCAL Sample Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1254332#M17872</link>
      <description>&lt;P&gt;Hi there&lt;BR /&gt;&lt;BR /&gt;Thanks for your response. I already had the OS installed. the difference was the example was look for 88 and the OS 103 that i had installed has the plugins for OS_TS ending with 92. So again i updated the .pref/xdm files to point to 92 and that error vanished.&lt;BR /&gt;&lt;BR /&gt;So looks like the example delivered with MCAP 105 is not updated from 103 for MCAL and from 88 to 92 for OS. It would be great if this is updated and the procedure is made simpler.&lt;BR /&gt;&lt;BR /&gt;Thanks but for your prompt replies. I was able to load the example project now successfully.&lt;BR /&gt;Now i understand that i need to generate the code and then take it back into my C IDE and compile the same and build my application on top of this based on the BSW, RTE and OS Stack.&lt;BR /&gt;&lt;BR /&gt;Is that also available in the EB Tresos 14.2 or this version of EB Tresos is designed only for MCAL generation.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Malai&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 15:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1254332#M17872</guid>
      <dc:creator>cmalai</dc:creator>
      <dc:date>2021-03-30T15:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to import NXP Autosar MCAL Sample Application</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1254763#M17876</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If I understand correctly your question, then we don't provide the RTE and OS stack, so it's pretty much depended on the 3rd party who provides these package to make their RTE and OS stack to compatible with EB Tresos 14.2.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Nam&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 07:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Unable-to-import-NXP-Autosar-MCAL-Sample-Application/m-p/1254763#M17876</guid>
      <dc:creator>namnguyenviet</dc:creator>
      <dc:date>2021-03-31T07:11:06Z</dc:date>
    </item>
  </channel>
</rss>