<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5744P reset escalation</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246345#M17697</link>
    <description>&lt;P&gt;Actually with S32DS it may be pretty simple to connect:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/MPC5748G-Reset-escalation-PEMicro-Multilink-FX/m-p/951223#M14328" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/MPC5748G-Reset-escalation-PEMicro-Multilink-FX/m-p/951223#M14328&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Check following thread&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 10:12:47 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2021-03-16T10:12:47Z</dc:date>
    <item>
      <title>MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246142#M17689</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While trying to setup the Online BIST I managed to input a wrong clock divider (I used an even value instead of odd) and now my board entered reset escalation. After that I wasn't able to connect with the debugger anymore. Is it possible to get out of that state now, and how?&lt;BR /&gt;On the other hand, is it possible that it's really that easy to kill the microcontroller with one bad write to a register?&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Vladimir&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 08:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246142#M17689</guid>
      <dc:creator>VladiKn</dc:creator>
      <dc:date>2021-03-16T08:20:38Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246294#M17695</link>
      <description>&lt;P&gt;Hi, The solution is to stop the core just after power-on-reset, attach by debugger and erase MCU/reload the code.&lt;BR /&gt;With TRACE32 it can be done by “Halt core at power-on reset” feature (Select in the menu: MPC5XXX - Tools - Halt core at power-on reset.).&lt;/P&gt;
&lt;P&gt;It can be done with PeMicro as well, but procedure is no so simple. Which debugger you are using?&lt;/P&gt;
&lt;P&gt;You cannot bricked out the MCU by simple register write, it would have to be some NVM programming as DCF records.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 09:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246294#M17695</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-03-16T09:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246324#M17696</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the quick response. Currently I am using PEMicro. Do you have an example how to do it?&lt;BR /&gt;In the MC_CGM_SC_DC0 register I put a value of 0x4 in the DIV field and my application crashed. After that I was no longer able to connect to the board. So I don't know what else could it be.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 09:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246324#M17696</guid>
      <dc:creator>VladiKn</dc:creator>
      <dc:date>2021-03-16T09:47:10Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246345#M17697</link>
      <description>&lt;P&gt;Actually with S32DS it may be pretty simple to connect:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/MPC5748G-Reset-escalation-PEMicro-Multilink-FX/m-p/951223#M14328" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/MPC5748G-Reset-escalation-PEMicro-Multilink-FX/m-p/951223#M14328&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Check following thread&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 10:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246345#M17697</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-03-16T10:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246436#M17702</link>
      <description>&lt;P&gt;Sorry I gave you the wrong information. Actually I use the OpenSDA port for debugging.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 12:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1246436#M17702</guid>
      <dc:creator>VladiKn</dc:creator>
      <dc:date>2021-03-16T12:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P reset escalation</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1247264#M17710</link>
      <description>&lt;P&gt;I believe in this context it should be pretty much the same.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 13:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5744P-reset-escalation/m-p/1247264#M17710</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-03-17T13:03:22Z</dc:date>
    </item>
  </channel>
</rss>