<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Read/write non volatile variable</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233427#M17397</link>
    <description>&lt;P&gt;Thanks for the answer,&lt;/P&gt;&lt;P&gt;I'm trying to define a variable wich I can modify by the main program and the changes of this variable save in all power on - off process or reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But I don't get this result. I have this try program to function like a toogle the variable but when I reset the hardware I don't see the expected process.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;if (startup_state != 0xAA)&lt;BR /&gt;{&lt;BR /&gt;startup_state = 0xAA;&lt;BR /&gt;..............&lt;BR /&gt;}&lt;BR /&gt;else&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;startup_state = 0x00;&lt;BR /&gt;...............................&lt;BR /&gt;}&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When you say:&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;SPAN&gt;Permanent copy of data lives in flash, but gets loaded to RAM on boot.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Software uses and modifies the RAM version.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Changes get written back to flash under software control.&lt;/SPAN&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&lt;SPAN&gt;This mean that I need to save the value before the sistem reset?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I need this variable with the last value all time, because the system can be power off anytime&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 19 Feb 2021 07:49:28 GMT</pubDate>
    <dc:creator>Ekaitz</dc:creator>
    <dc:date>2021-02-19T07:49:28Z</dc:date>
    <item>
      <title>Read/write non volatile variable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1232983#M17388</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm doin a proyect whit the micro MPC 5744P with GNU toolchain.&lt;/P&gt;&lt;P&gt;I'm triyin to define a variable that can write and read but not initialize in all the power on of.&lt;/P&gt;&lt;P&gt;I'm tray to define a variable in liker scrip but I dont get the espected results&lt;/P&gt;&lt;P&gt;My example is this:&lt;/P&gt;&lt;P&gt;Linker script&lt;/P&gt;&lt;P&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt;flash_rchw : org = 0x00F98000, len = 4&lt;BR /&gt;cpu0_reset_vec : org = 0x00F98004, len = 4&lt;/P&gt;&lt;P&gt;m_my_flash : org = 0x01000000, len = 4&lt;BR /&gt;m_text : org = 0x01000004, len = 2048K - 4&lt;/P&gt;&lt;P&gt;m_my_ram : org = 0x40000000, len = 4&lt;BR /&gt;m_data : org = 0x40000004, len = 384K - 4&lt;/P&gt;&lt;P&gt;local_dmem :org = 0x50800000, len = 64K&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;SECTIONS&lt;BR /&gt;{&lt;BR /&gt;...............&lt;BR /&gt;.startup_state_sect ORIGIN(m_my_ram) :&lt;BR /&gt;{&lt;BR /&gt;KEEP (*(.startup_state_sect))&lt;BR /&gt;} &amp;gt; m_my_ram AT &amp;gt; m_my_flash&lt;BR /&gt;......................&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Code:&lt;/P&gt;&lt;P&gt;uint32_t __attribute__((__section__(".startup_state_sect"))) startup_state;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 15:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1232983#M17388</guid>
      <dc:creator>Ekaitz</dc:creator>
      <dc:date>2021-02-18T15:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: Read/write non volatile variable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233003#M17389</link>
      <description>&lt;P&gt;&amp;nbsp;I am not sure I fully understand your question, but I will try.&lt;/P&gt;&lt;P&gt;How is this variable going to be non-volatile? Your linker script is creating a variable that operates from RAM but gets initialised by startup code to an initial value from flash.&lt;BR /&gt;The conventional approaches I can think of.&lt;/P&gt;&lt;P&gt;1. semi non volatile - store it in a standby RAM section (if available on 5744P)&lt;/P&gt;&lt;P&gt;2. Permanent copy of data lives in flash, but gets loaded to RAM on boot.&lt;BR /&gt;Software uses and modifies the RAM version.&lt;BR /&gt;Changes get written back to flash under software control.&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 16:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233003#M17389</guid>
      <dc:creator>jamesmurray</dc:creator>
      <dc:date>2021-02-18T16:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: Read/write non volatile variable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233015#M17390</link>
      <description>&lt;P&gt;It is typical to define non-volatile data as const storage class. It can be changed by flash reprogramming.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 16:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233015#M17390</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-02-18T16:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: Read/write non volatile variable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233427#M17397</link>
      <description>&lt;P&gt;Thanks for the answer,&lt;/P&gt;&lt;P&gt;I'm trying to define a variable wich I can modify by the main program and the changes of this variable save in all power on - off process or reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But I don't get this result. I have this try program to function like a toogle the variable but when I reset the hardware I don't see the expected process.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;if (startup_state != 0xAA)&lt;BR /&gt;{&lt;BR /&gt;startup_state = 0xAA;&lt;BR /&gt;..............&lt;BR /&gt;}&lt;BR /&gt;else&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;startup_state = 0x00;&lt;BR /&gt;...............................&lt;BR /&gt;}&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When you say:&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;SPAN&gt;Permanent copy of data lives in flash, but gets loaded to RAM on boot.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Software uses and modifies the RAM version.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Changes get written back to flash under software control.&lt;/SPAN&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&lt;SPAN&gt;This mean that I need to save the value before the sistem reset?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I need this variable with the last value all time, because the system can be power off anytime&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 07:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233427#M17397</guid>
      <dc:creator>Ekaitz</dc:creator>
      <dc:date>2021-02-19T07:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Read/write non volatile variable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233689#M17402</link>
      <description>&lt;P&gt;In my previous message I wrote about using flash memory for storage. Actually, that's not a good idea to do this on the flash within the device for two reasons:&lt;BR /&gt;1. The flash has a limited number of write cycles and constant use will wear it out.&lt;BR /&gt;2. If the "system can be power off anytime" your flash write could be interrupted and left in an unknown state.&lt;/P&gt;&lt;P&gt;If you really need this, then perhaps battery backed-up RAM is a better idea. I looked and it seems that the 5744P does not have standby RAM. (The 5746R does.)&lt;BR /&gt;So maybe some external RAM with battery backup. You would need to use two regions and alternate between them. Otherwise if power is lost at the time you are writing you will get unknown behaviour.&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 14:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Read-write-non-volatile-variable/m-p/1233689#M17402</guid>
      <dc:creator>jamesmurray</dc:creator>
      <dc:date>2021-02-19T14:32:20Z</dc:date>
    </item>
  </channel>
</rss>