<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックCAN question</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CAN-question/m-p/1193708#M16784</link>
    <description>&lt;P&gt;&lt;SPAN&gt;MPC5744 + FS6510CAE.when using SBC's CAN transceiver, it will cause the chip to reset. What is the reason? I tested that the current will rise from 90mA to 700mA during data transmission using the CAN transceiver&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And when the core voltage is calculated according to the theory and the resistance is configured, it is found that the theoretical value of 1.25V is less than the actual 1.30V.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Dec 2020 05:41:23 GMT</pubDate>
    <dc:creator>kai5</dc:creator>
    <dc:date>2020-12-04T05:41:23Z</dc:date>
    <item>
      <title>CAN question</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-question/m-p/1193708#M16784</link>
      <description>&lt;P&gt;&lt;SPAN&gt;MPC5744 + FS6510CAE.when using SBC's CAN transceiver, it will cause the chip to reset. What is the reason? I tested that the current will rise from 90mA to 700mA during data transmission using the CAN transceiver&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And when the core voltage is calculated according to the theory and the resistance is configured, it is found that the theoretical value of 1.25V is less than the actual 1.30V.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Dec 2020 05:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-question/m-p/1193708#M16784</guid>
      <dc:creator>kai5</dc:creator>
      <dc:date>2020-12-04T05:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: CAN question</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CAN-question/m-p/1193761#M16785</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you check on scope if there wasn't any drop voltages when the reset occurred?&lt;/P&gt;
&lt;P&gt;You can also check the ME module RGM [FES and DES] registers for its content after reset. There are logged reset sources.&lt;/P&gt;
&lt;P&gt;Also you can check FCCU module NCFS flags for issue root cause (remember to set 0xA to the Control (FCCU_CTRL) OPS field).&lt;/P&gt;
&lt;P&gt;If possible share them with me so I can see where is the issue.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 04 Dec 2020 07:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CAN-question/m-p/1193761#M16785</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-12-04T07:29:34Z</dc:date>
    </item>
  </channel>
</rss>