<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RAppID Boot Loader for Linux in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/1178379#M16636</link>
    <description>&lt;P&gt;Hi Stanish,&lt;/P&gt;&lt;P&gt;Due to CAN bus hardware limitation, I'd like to write a small software to support CAN bootloader via PCAN. Could you please provide CCP CRO and DTO ID? thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 05 Nov 2020 01:41:36 GMT</pubDate>
    <dc:creator>Wally0258</dc:creator>
    <dc:date>2020-11-05T01:41:36Z</dc:date>
    <item>
      <title>RAppID Boot Loader for Linux</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779383#M11339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I may need to update the firmware in a MPC5643L remotely. &amp;nbsp;LINFlex_0's UART is connected to an embedded linux board. &amp;nbsp;Does a linux command line version of the RAppID boot loader exist? &amp;nbsp;I suspect that I might have to write one myself based on the description of the Boot Assist Module in the reference manual and maybe snooping the serial port of the Windows CLI version. &amp;nbsp;Some source code of the existing versions would come in handy, is any obtainable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Shaun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 01:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779383#M11339</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2017-11-16T01:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: RAppID Boot Loader for Linux</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779384#M11340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As far as i know there is no Linux version of RAppid Bootloader. The PC-side application is written in C# and currently it support just Windows platform.&lt;/P&gt;&lt;P&gt;Unfortunately we do not provide a source code.&lt;/P&gt;&lt;P&gt;It's based on CCP protocol (&lt;A class="link-titled" href="https://automotivetechis.files.wordpress.com/2012/06/ccp211.pdf" title="https://automotivetechis.files.wordpress.com/2012/06/ccp211.pdf"&gt;https://automotivetechis.files.wordpress.com/2012/06/ccp211.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See more details about Rappid Bootloader here:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/video/overview-of-rappid-bootloader:WBNR-FTF2014-AUT-F0014-B-VID" title="https://www.nxp.com/video/overview-of-rappid-bootloader:WBNR-FTF2014-AUT-F0014-B-VID"&gt;Overview of RAppID Bootloader|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 12:19:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779384#M11340</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-11-16T12:19:51Z</dc:date>
    </item>
    <item>
      <title>Re: RAppID Boot Loader for Linux</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779385#M11341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stanislav,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't think I'd have much joy on the source code or linux front. &amp;nbsp;Thanks very much for your links, especially to the CCP protocol, that is very useful - I am not in the automotive sector and I did not know it existed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Shaun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Nov 2017 00:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779385#M11341</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2017-11-17T00:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: RAppID Boot Loader for Linux</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779386#M11342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Shaun James wrote:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Stanislav,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't think I'd have much joy on the source code or linux front. &amp;nbsp;Thanks very much for your links, especially to the CCP protocol, that is very useful - I am not in the automotive sector and I did not know it existed.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, Shaun&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;You may get lucky looking at the pyccp module:&amp;nbsp;&lt;A class="link-titled" href="https://github.com/pySART/pyccp" title="https://github.com/pySART/pyccp"&gt;GitHub - pySART/pyccp: ASAM CAN Calibration Protocol for Python&lt;/A&gt;&amp;nbsp;&lt;A class="link-titled" href="https://github.com/pySART/pyccp/blob/master/setup.py" title="https://github.com/pySART/pyccp/blob/master/setup.py"&gt;https://github.com/pySART/pyccp/blob/master/setup.py&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Dec 2019 17:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/779386#M11342</guid>
      <dc:creator>jfrey</dc:creator>
      <dc:date>2019-12-15T17:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: RAppID Boot Loader for Linux</title>
      <link>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/1178379#M16636</link>
      <description>&lt;P&gt;Hi Stanish,&lt;/P&gt;&lt;P&gt;Due to CAN bus hardware limitation, I'd like to write a small software to support CAN bootloader via PCAN. Could you please provide CCP CRO and DTO ID? thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Nov 2020 01:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/RAppID-Boot-Loader-for-Linux/m-p/1178379#M16636</guid>
      <dc:creator>Wally0258</dc:creator>
      <dc:date>2020-11-05T01:41:36Z</dc:date>
    </item>
  </channel>
</rss>