<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Problem facing while working with SRAM.</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461630#M1649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Multiplexed and Non-Multiplexed modes have to do with the total number of pins used for the interface. In Non-multiplexed mode Data and Address have dedicated pins.&lt;/P&gt;&lt;P&gt;In multiplexed mode the address is driven on the data pins during the address Phase hence lesser number of pins are required.&lt;/P&gt;&lt;P&gt;This Application note might help you understand better: &lt;A href="http://www.nxp.com/files/32bit/doc/app_note/AN3854.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN3854.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 May 2016 06:52:38 GMT</pubDate>
    <dc:creator>ameyaranade</dc:creator>
    <dc:date>2016-05-30T06:52:38Z</dc:date>
    <item>
      <title>Problem facing while working with SRAM.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461628#M1647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am working on SRAM using EBI communication. I am trying to write a bunch(1kilo bytes) of data to it. In that whole data write, two to three bytes of data is failing to write. As this is a parallel communication, i am unable to track the communication. I want to know, what are the major issue's we may face while working with EBI. And also i didnt understood nonmultiplex/multiplex mode. Did any having the data which explains this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 May 2016 15:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461628#M1647</guid>
      <dc:creator>ravitejaveeraga</dc:creator>
      <dc:date>2016-05-29T15:41:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing while working with SRAM.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461629#M1648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please clarify used MCU and whether you are using EVB or your own prototype board. Also I would to know used configuration and detailed description of the issue. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 06:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461629#M1648</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-05-30T06:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing while working with SRAM.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461630#M1649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Multiplexed and Non-Multiplexed modes have to do with the total number of pins used for the interface. In Non-multiplexed mode Data and Address have dedicated pins.&lt;/P&gt;&lt;P&gt;In multiplexed mode the address is driven on the data pins during the address Phase hence lesser number of pins are required.&lt;/P&gt;&lt;P&gt;This Application note might help you understand better: &lt;A href="http://www.nxp.com/files/32bit/doc/app_note/AN3854.pdf"&gt;http://www.nxp.com/files/32bit/doc/app_note/AN3854.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 06:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461630#M1649</guid>
      <dc:creator>ameyaranade</dc:creator>
      <dc:date>2016-05-30T06:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing while working with SRAM.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461631#M1650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) MCU is MPC5777C. &lt;/P&gt;&lt;P&gt;2) Using my own prototype board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCR&amp;nbsp;&amp;nbsp; = 0x00000801&lt;/P&gt;&lt;P&gt;BMCR = 0x0000FF80&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59398iB249F02F105162BD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I followed this configuration.&lt;/P&gt;&lt;P&gt;And below are the some of the configuration.&lt;/P&gt;&lt;P&gt;MCR&amp;nbsp; = 0x00000801&lt;/P&gt;&lt;P&gt;BMCR&amp;nbsp; = 0x0000FF80&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 08:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461631#M1650</guid>
      <dc:creator>ravitejaveeraga</dc:creator>
      <dc:date>2016-05-30T08:46:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing while working with SRAM.</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461632#M1651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could I see scheme of connection? Could I see piece of code using for EBI access? Have you tried to play with timing setup? Do you have more pieces of your prototype board? Still same issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 11:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Problem-facing-while-working-with-SRAM/m-p/461632#M1651</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2016-06-03T11:52:49Z</dc:date>
    </item>
  </channel>
</rss>