<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5746R eDMA register can't  write or read in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1094164#M16461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;The debugger is telling you that in order to change register values, your code cannot run.&lt;/P&gt;&lt;P&gt;Stop the code and then change the values.&lt;/P&gt;&lt;P&gt;Or use debugger which is capable of this operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 May 2020 05:17:22 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2020-05-04T05:17:22Z</dc:date>
    <item>
      <title>MPC5746R eDMA register can't  write or read</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1094163#M16460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;I is&amp;nbsp; debuging MPC5746R for DMA. But When I use S32DS debug MPC5746R, the DMA register cannot be written or read. The debuger is USB Multilink Universal.&lt;/P&gt;&lt;P&gt;code:&lt;/P&gt;&lt;P&gt;DMA_0.TCD[7].WORD_1.B.SMOD = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_1.B.SSIZE = 0x2; /* 32-bit */&lt;BR /&gt; DMA_0.TCD[7].WORD_1.B.DMOD = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_1.B.DSIZE = 0x2; /* 32-bit */&lt;BR /&gt; DMA_0.TCD[7].WORD_1.B.SOFF = 0x4; //Source address signed offset&lt;BR /&gt; DMA_0.TCD[7].WORD_2.NBYTES.B.NBYTES = 64; /* Minor Byte Transfer Count (16x32-bits)/8=64byte */&lt;BR /&gt; DMA_0.TCD[7].WORD_3.B.SLAST = -64;&lt;BR /&gt; DMA_0.TCD[7].WORD_4.B.DADDR = (uint32)&amp;amp;DMA_save_result0;&lt;BR /&gt; DMA_0.TCD[7].WORD_5.B.CITER_E_LINK = 0; //The channel-to-channel linking is disabled&lt;BR /&gt; //DMA_0.TCD[0].WORD_5.B.LINKCH_CITER = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_5.B.CITER = 1;&lt;BR /&gt; DMA_0.TCD[7].WORD_5.B.DOFF = 0x4; //Destination address signed offset&lt;BR /&gt; DMA_0.TCD[7].WORD_6.B.DLAST_SGA= -64;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.BITER = 1; //&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.BITER_E_LINK = 0; //0=The channel-to-channel linking is disabled&lt;BR /&gt; //DMA_0.TCD[0].WORD_7.B.BITER_BITER_LINKCH = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.BWC = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.MAJOR_LINKCH = 1; /* Link to channel 1 */&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.MAJOR_E_LINK = 1; /* Enable channel linking */&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.E_SG = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.DREQ = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.INT_HALF = 0;&lt;BR /&gt; DMA_0.TCD[7].WORD_7.B.INT_MAJOR = 0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error:&lt;/P&gt;&lt;P&gt;MPC574xR Device detected. &lt;BR /&gt;Unable to go into background mode.&lt;/P&gt;&lt;P&gt;PE-ERROR: Warning. Can't read registers while part is running.&lt;BR /&gt;PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)&lt;BR /&gt;PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to access DMA_0 register&amp;nbsp; other Byte,the result is same.&lt;/P&gt;&lt;P&gt;why can&lt;SPAN&gt;'t&amp;nbsp; access DMA_0 register,i&amp;nbsp; need&amp;nbsp; help&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f; "&gt;Kind regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f; "&gt;CGJ&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 07:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1094163#M16460</guid>
      <dc:creator>冠军蔡</dc:creator>
      <dc:date>2020-04-29T07:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R eDMA register can't  write or read</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1094164#M16461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;The debugger is telling you that in order to change register values, your code cannot run.&lt;/P&gt;&lt;P&gt;Stop the code and then change the values.&lt;/P&gt;&lt;P&gt;Or use debugger which is capable of this operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2020 05:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1094164#M16461</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-05-04T05:17:22Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5746R eDMA register can't  write or read</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1203716#M16934</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149979"&gt;@冠军蔡&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do you solve this problem? I encounter a similar problem.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 14:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5746R-eDMA-register-can-t-write-or-read/m-p/1203716#M16934</guid>
      <dc:creator>vegetarian1</dc:creator>
      <dc:date>2020-12-23T14:52:53Z</dc:date>
    </item>
  </channel>
</rss>