<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 How to use Overlay RAM?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/How-to-use-Overlay-RAM/m-p/461545#M1643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone share use the reference code about how to use Qorivva 57XX Overlay RAM? If the target MCU is Rainer is best.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jan 2016 07:47:20 GMT</pubDate>
    <dc:creator>hongpingxu-b364</dc:creator>
    <dc:date>2016-01-25T07:47:20Z</dc:date>
    <item>
      <title>How to use Overlay RAM?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-use-Overlay-RAM/m-p/461545#M1643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone share use the reference code about how to use Qorivva 57XX Overlay RAM? If the target MCU is Rainer is best.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 07:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-use-Overlay-RAM/m-p/461545#M1643</guid>
      <dc:creator>hongpingxu-b364</dc:creator>
      <dc:date>2016-01-25T07:47:20Z</dc:date>
    </item>
    <item>
      <title>Re: How to use Overlay RAM?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-to-use-Overlay-RAM/m-p/461546#M1644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you need to configure the relevant registers to remap a flash location to internal overlay RAM:&lt;/P&gt;&lt;P&gt;PFLASH_PFCRDn_Word1&lt;/P&gt;&lt;P&gt;PFLASH_PFCRDn_Word2&lt;/P&gt;&lt;P&gt;PFLASH_PFCRDn_Word3&lt;/P&gt;&lt;P&gt;User need to refer the Flash Mirrored location (for example 0x08F9_C000) as the Logical StartAddress not the actual Flash address. Overlay RAM location should be used as the Physical StartAddress (for example internal Overlay RAM 0x0D00_0000 – I’m talking about MPC5746R, it can be different on other devices). Please refer the Memory Map excel to find out which areas can be overlayed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then enable the remapping by Platform Flash Remap Descriptor Enable Register and by Platform Flash Remap Control Register. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initial data should be copied from flash to overlay SRAM by user. Once the calibration is done, the data should be programmed back to flash by user - this is not done automatically, of course. &lt;/P&gt;&lt;P&gt;Overlay SRAM is normally used for system development purposes only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 11:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-to-use-Overlay-RAM/m-p/461546#M1644</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-01-27T11:35:18Z</dc:date>
    </item>
  </channel>
</rss>