<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: DCF Clients - Program - MPC5746R</title>
    <link>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079628#M16237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry a mistake, is 8 bytes not 4 bytes. With 4 Bytes it&amp;nbsp;will be an error program in the fourth program of the phrase of 32 bytes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2020 17:40:03 GMT</pubDate>
    <dc:creator>demian91</dc:creator>
    <dc:date>2020-05-27T17:40:03Z</dc:date>
    <item>
      <title>DCF Clients - Program - MPC5746R</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079625#M16234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi is possible to program the UTEST sector, in my case, starts from 0x400310, program&amp;nbsp;with code for each 8 bytes of DCF Client without problems with the OTP. i understand that once you program a byte, is for ever so i want to be sure. I test in other sector&amp;nbsp;that if i only program what the necesary space (to the end of DCF Clients) it can be continued after.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 01:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079625#M16234</guid>
      <dc:creator>demian91</dc:creator>
      <dc:date>2020-05-27T01:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: DCF Clients - Program - MPC5746R</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079626#M16235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am quite confused by your explanation.&lt;/P&gt;&lt;P&gt;I will summarize it.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;is possible to program the UTEST sector, in my case, starts from 0x400310, program&amp;nbsp;with code for each 8 bytes of DCF Client without problems with the OTP.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Yes you can program this UTEST space with&amp;nbsp; 64-bit DCF clients.&lt;/P&gt;&lt;P&gt;This area is OTP so you can program it only once. (it means each bit can be programmed only once)&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;i understand that once you program a byte, is for ever so i want to be sure.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Yes, that is what OTP means.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;I test in other sector&amp;nbsp;that if i only program what the necesary space (to the end of DCF Clients) it can be continued after.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I do not understand this sentence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 06:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079626#M16235</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-05-27T06:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: DCF Clients - Program - MPC5746R</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079627#M16236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the third sentence i say that i test that i can program in phrases of 4 bytes so it wouldn't be a problem because i understand that the minimum sector to be programmed is 32 bytes. I was afraid that if i program 4 bytes, others bytes is going to be programmed so i couldn't program the next DCF Clients in the future. Is i program for example 0xFFFFFFFF in a location with the same value 0xFFFFFFFF, it programs that once for ever or in reality i can always program this location with bits 1 to 0?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 15:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079627#M16236</guid>
      <dc:creator>demian91</dc:creator>
      <dc:date>2020-05-27T15:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: DCF Clients - Program - MPC5746R</title>
      <link>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079628#M16237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry a mistake, is 8 bytes not 4 bytes. With 4 Bytes it&amp;nbsp;will be an error program in the fourth program of the phrase of 32 bytes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 17:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/DCF-Clients-Program-MPC5746R/m-p/1079628#M16237</guid>
      <dc:creator>demian91</dc:creator>
      <dc:date>2020-05-27T17:40:03Z</dc:date>
    </item>
  </channel>
</rss>