<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックMPC5777M errata e048</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-errata-e048/m-p/460148#M1601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using LVDS pair pins on MPC5777M. I found things relating as following in the IO definition spreadsheet attached to MPC577M reference manual Rev4 downloaded from Freescale website.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"To select the LVDS interface, select the function with the SSS field in the MSCR of the positive terminal, &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;and the appropriate LVDS option in the ODC (output) or ILS (input) fields in the MSCR of both terminals.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; Note that these bits have no effect on cut1 of the device (see errata e048)."&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, the configuration for these pair pins do not work properly.&lt;/P&gt;&lt;P&gt;So I would like to ask for errata e048 in case It could help to verify the issue.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Chuong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Dec 2015 08:28:09 GMT</pubDate>
    <dc:creator>chuongvo</dc:creator>
    <dc:date>2015-12-03T08:28:09Z</dc:date>
    <item>
      <title>MPC5777M errata e048</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-errata-e048/m-p/460148#M1601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using LVDS pair pins on MPC5777M. I found things relating as following in the IO definition spreadsheet attached to MPC577M reference manual Rev4 downloaded from Freescale website.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"To select the LVDS interface, select the function with the SSS field in the MSCR of the positive terminal, &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;and the appropriate LVDS option in the ODC (output) or ILS (input) fields in the MSCR of both terminals.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; Note that these bits have no effect on cut1 of the device (see errata e048)."&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, the configuration for these pair pins do not work properly.&lt;/P&gt;&lt;P&gt;So I would like to ask for errata e048 in case It could help to verify the issue.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Chuong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 08:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-errata-e048/m-p/460148#M1601</guid>
      <dc:creator>chuongvo</dc:creator>
      <dc:date>2015-12-03T08:28:09Z</dc:date>
    </item>
  </channel>
</rss>