<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5606B microntroller compatibility with SPC560B60L7 in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039063#M15564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Considering what we are offering on our web as available-&lt;/P&gt;&lt;P&gt;Mentioned SPC5606BF1VLU6 has smaller temperature range -40 to 105 °C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPC5606BK0MLU6 could be better option, it has the parameters, but it is slightly different device. Differences are fully described in the following appnote:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4477.pdf" title="https://www.nxp.com/docs/en/application-note/AN4477.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4477.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the same package all devices should be pin-to-pin compatible, regarding mask set or device revision, I cannot comment, because I don't know ST part.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2020 19:05:09 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2020-07-02T19:05:09Z</dc:date>
    <item>
      <title>MPC5606B microntroller compatibility with SPC560B60L7</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039060#M15561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm doing a HW rework&amp;nbsp;design about a board that use the microcontroller&amp;nbsp;SPC560B60L7 of STMicroelectronics. I want update the design using a NXP microcontroller. I have seen that this device is similar to the MPC5606B, but I would like to know if the 2&amp;nbsp;IC are pin-to-pin compatible. In particular, is it possible to replace one component with the other one without modify the electrical connections already present on the board?&lt;/P&gt;&lt;P&gt;The complete part number identified are: SPC5606BF1VLU6&amp;nbsp;(of NXP) and SPC560B64L7C6E0X (of ST).&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 07:58:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039060#M15561</guid>
      <dc:creator>andrearicca</dc:creator>
      <dc:date>2020-06-29T07:58:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B microntroller compatibility with SPC560B60L7</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039061#M15562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, could you provide MIDR registers' content ot the ST part?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2020 16:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039061#M15562</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2020-06-30T16:04:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B microntroller compatibility with SPC560B60L7</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039062#M15563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Actually I can not read the MCU registers. The complete ST part number used is&amp;nbsp;SPC560B60L7C6E0Y:&lt;/P&gt;&lt;P&gt;- Flash memory 1MB&lt;/P&gt;&lt;P&gt;- Package LQPF176&lt;/P&gt;&lt;P&gt;-&amp;nbsp;Execution speed 64MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 08:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039062#M15563</guid>
      <dc:creator>andrearicca</dc:creator>
      <dc:date>2020-07-01T08:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B microntroller compatibility with SPC560B60L7</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039063#M15564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Considering what we are offering on our web as available-&lt;/P&gt;&lt;P&gt;Mentioned SPC5606BF1VLU6 has smaller temperature range -40 to 105 °C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPC5606BK0MLU6 could be better option, it has the parameters, but it is slightly different device. Differences are fully described in the following appnote:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4477.pdf" title="https://www.nxp.com/docs/en/application-note/AN4477.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4477.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the same package all devices should be pin-to-pin compatible, regarding mask set or device revision, I cannot comment, because I don't know ST part.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 19:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-microntroller-compatibility-with-SPC560B60L7/m-p/1039063#M15564</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2020-07-02T19:05:09Z</dc:date>
    </item>
  </channel>
</rss>