<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5566 clkout frequency during flashloading</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-clkout-frequency-during-flashloading/m-p/1037672#M15541</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Franz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first, clock frequency depends on your configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98882i07D0F86FE07B0E7A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;For example, if&amp;nbsp; you use default configuration and if you have 8MHz crystal, then system clock is 12MHz (see default PLL settings).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Clocks configuration can be changed in *.cmm scripts if needed. So, you should check which scripts you use. If there's no additional PLL configuration, then default clocks are used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 08:44:12 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2020-03-18T08:44:12Z</dc:date>
    <item>
      <title>MPC5566 clkout frequency during flashloading</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-clkout-frequency-during-flashloading/m-p/1037671#M15540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a question to the MPC5566.&lt;/P&gt;&lt;P&gt;What is the clkout frequency during flashing the internal flash via lauterbach debugger?&lt;/P&gt;&lt;P&gt;greetings&lt;/P&gt;&lt;P&gt;Franz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2020 09:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5566-clkout-frequency-during-flashloading/m-p/1037671#M15540</guid>
      <dc:creator>franzstemmer</dc:creator>
      <dc:date>2020-03-17T09:39:09Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5566 clkout frequency during flashloading</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5566-clkout-frequency-during-flashloading/m-p/1037672#M15541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Franz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;first, clock frequency depends on your configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98882i07D0F86FE07B0E7A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;For example, if&amp;nbsp; you use default configuration and if you have 8MHz crystal, then system clock is 12MHz (see default PLL settings).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Clocks configuration can be changed in *.cmm scripts if needed. So, you should check which scripts you use. If there's no additional PLL configuration, then default clocks are used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 08:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5566-clkout-frequency-during-flashloading/m-p/1037672#M15541</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-03-18T08:44:12Z</dc:date>
    </item>
  </channel>
</rss>