<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5604E - Data via BroadR-Reach</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458599#M1544</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As far as I know I can’t reprogram much without buying the Freescale Autosar OS. Is this correct? The only other thing a probably could do is flashing the AVBproject instead of the UDP one, but viewing the videostream via AVB will be very difficult I guess.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jan 2016 12:48:11 GMT</pubDate>
    <dc:creator>thiesteichmann</dc:creator>
    <dc:date>2016-01-06T12:48:11Z</dc:date>
    <item>
      <title>MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458596#M1541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've connected my MPC5604E to a technica engineering Media Gateway which is connected to my PC. If the MPC5604E and the Media Gateway are connected via Ethernet, video data which can be viewed with the VLC Player is transmitted. But if i use a BroadR-Reach cable to connect the MPC5604E to the Media Gateway, it seems like no real data is transmitted, only an idle signal of alternating -1 V and 1 V levels. Can someone please tell me what i have to do to enable transmitting via BroadR-Reach?Any help would be greatly appreciated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 12:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458596#M1541</guid>
      <dc:creator>thiesteichmann</dc:creator>
      <dc:date>2015-12-03T12:37:05Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458597#M1542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bump&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone an idea how to do this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 11:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458597#M1542</guid>
      <dc:creator>thiesteichmann</dc:creator>
      <dc:date>2016-01-04T11:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458598#M1543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thies,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you re-program the firmware which can support BroadR-Reach phy?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 01:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458598#M1543</guid>
      <dc:creator>kentlin</dc:creator>
      <dc:date>2016-01-06T01:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458599#M1544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As far as I know I can’t reprogram much without buying the Freescale Autosar OS. Is this correct? The only other thing a probably could do is flashing the AVBproject instead of the UDP one, but viewing the videostream via AVB will be very difficult I guess.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 12:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458599#M1544</guid>
      <dc:creator>thiesteichmann</dc:creator>
      <dc:date>2016-01-06T12:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458600#M1545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please downlaod the MPC5604E demo project from&lt;/P&gt;&lt;P&gt;&lt;A class="dtmAssetClick" data-dtmassettype="Download" data-dtmname="Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries" href="https://www.nxp.com/webapp/Download?colCode=FSL-REFKIT-MPC564E&amp;amp;appType=license&amp;amp;location=null" target="_blank"&gt;Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries&lt;/A&gt;&lt;SPAN class="small-rev"&gt; (REV 0.8.2)&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;There is a compiled firware " intapp_udp_br.elf " which can support BroadR-Reach Phy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you don't need to have Autosar OS to re-compile the project, if you don't want to modify the source file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Kent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jan 2016 05:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458600#M1545</guid>
      <dc:creator>kentlin</dc:creator>
      <dc:date>2016-01-07T05:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458601#M1546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much. It works now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 13:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458601#M1546</guid>
      <dc:creator>thiesteichmann</dc:creator>
      <dc:date>2016-01-12T13:26:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458602#M1547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I only want to change the ip addresses, cause I want to use 4 cameras simultaneously now. So guess I need to change the ip address in the control_app.c and recompile the project. What files do I need to do this? It says at first that the os.h is missing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Thies&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 16:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458602#M1547</guid>
      <dc:creator>thiesteichmann</dc:creator>
      <dc:date>2016-01-28T16:24:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604E - Data via BroadR-Reach</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458603#M1548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thies,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to re-compile the project, you will need the MPC5604E Autosar OS source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 06:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5604E-Data-via-BroadR-Reach/m-p/458603#M1548</guid>
      <dc:creator>kentlin</dc:creator>
      <dc:date>2016-02-01T06:32:50Z</dc:date>
    </item>
  </channel>
</rss>