<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: SPI interface issue with MPC5748G Devkit Revision D</title>
    <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021423#M15328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using pins of J3 port and the pins are,&lt;/P&gt;&lt;P&gt;2 - PA12 - Interrupt&lt;/P&gt;&lt;P&gt;5 - PF3 - Chip Select&lt;/P&gt;&lt;P&gt;7 - PF0 - MOSI&lt;/P&gt;&lt;P&gt;9 - PF1 - MISO&lt;/P&gt;&lt;P&gt;11 - PF2 - Clock Out&lt;/P&gt;&lt;P&gt;13 - GND - GND&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When compared the schematics for both revisions, there are no differences for the SPI connections i.e. for J3 connections. Only differences are for usage of latest MCU silicon, additional features of SD card etc for revision D board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to read device ID/signature of a flash memory connected over SPI interface. I have implemented a loop of 5 for reading this value. With rev B board, it works fine for all the 5 times but with rev D board, it works for the first time after power up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Dec 2019 06:20:58 GMT</pubDate>
    <dc:creator>sanjib_das</dc:creator>
    <dc:date>2019-12-17T06:20:58Z</dc:date>
    <item>
      <title>SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021421#M15326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have interfaced peripheral over SPI using J3 connector of MPC5748 DEVKIT. I am trying to read signature register from that peripheral. I observed erratic behavior with&amp;nbsp;Revision D board where I am able to read signature for first read operation after power up. It is failing for successive reads. If I power up the DEVKIT it works for first read operation.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I tried the same code with Revision B DEVKIT and it works fine for successive reads without needing multiple power up.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What could be the issue with Revision D DEVKIT? Are there any additional components required for SPI connection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Dec 2019 10:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021421#M15326</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2019-12-07T10:28:38Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021422#M15327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which pins do you use? Did you try to compare schematics for those 2 revisions?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;What does "failing for successive reads" means? You see no frame on SPI line, or just input data are wrong? What device is connected? Did you measure&amp;nbsp;SPI bus using scope/analyzer?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 08:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021422#M15327</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-12-12T08:46:43Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021423#M15328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using pins of J3 port and the pins are,&lt;/P&gt;&lt;P&gt;2 - PA12 - Interrupt&lt;/P&gt;&lt;P&gt;5 - PF3 - Chip Select&lt;/P&gt;&lt;P&gt;7 - PF0 - MOSI&lt;/P&gt;&lt;P&gt;9 - PF1 - MISO&lt;/P&gt;&lt;P&gt;11 - PF2 - Clock Out&lt;/P&gt;&lt;P&gt;13 - GND - GND&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When compared the schematics for both revisions, there are no differences for the SPI connections i.e. for J3 connections. Only differences are for usage of latest MCU silicon, additional features of SD card etc for revision D board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to read device ID/signature of a flash memory connected over SPI interface. I have implemented a loop of 5 for reading this value. With rev B board, it works fine for all the 5 times but with rev D board, it works for the first time after power up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 06:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021423#M15328</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2019-12-17T06:20:58Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021424#M15329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on those pins nothing is connected on both boards so no issue is expected. You can try to send SPI frames without memory connected.&lt;/P&gt;&lt;P&gt;The difference between MCU revisions are mentioned in errata documents&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/errata/MPC5748G_1N81M.pdf" title="https://www.nxp.com/docs/en/errata/MPC5748G_1N81M.pdf"&gt;https://www.nxp.com/docs/en/errata/MPC5748G_1N81M.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/errata/MPC5748G_0N78S.pdf" title="https://www.nxp.com/docs/en/errata/MPC5748G_0N78S.pdf"&gt;https://www.nxp.com/docs/en/errata/MPC5748G_0N78S.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 12:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021424#M15329</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-12-19T12:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021425#M15330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; tried loopback mode for SPI on both boards and it is working. But when external peripheral (memory) is connected, rev D board is not working correctly and Rev B is working. Observations are same as mentioned in earlier thread. With Rev D, I am really facing challenges for the stable operations over SPI. Look forward to your earliest help in this regards.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 06:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021425#M15330</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2020-01-13T06:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021426#M15331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;Your earliest reply is highly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 10:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021426#M15331</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2020-01-15T10:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021427#M15332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if SPI is working normally without memory connected, then this should not be issue of the MCU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What about a power supply? How is the power line of the memory connected? Are you able to power memory separately?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jan 2020 09:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021427#M15332</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-01-24T09:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021428#M15333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Memory has a separate power supply and I tried switching the same as well but observations remain same. It works with Rev B but fails with Rev D board.&lt;/P&gt;&lt;P&gt;As you mentioned, it may not be a problem with MCU-SPI engine but some thing with Rev D board.&lt;/P&gt;&lt;P&gt;Can you please help on priority as Rev B boards are not available and I am facing field failures with my proto design which uses Rev D board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for all your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,Sanjib&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 05:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021428#M15333</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2020-01-27T05:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021429#M15334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Waiting for your early reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,Sanjib&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 07:00:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021429#M15334</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2020-01-31T07:00:41Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021430#M15335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lets come full circle...&lt;/P&gt;&lt;P&gt;What exactly happen in the MCU after you successfully read first&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;device ID/signature of a flash memory?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Is the MCU hung somewhere in the code? Is the MCU reseted? If yes what is the reset source read from RGM module?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Is the MCU running SPI read functions, but no frame is visible on SPI bus, or you receive data but it is wrong?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 10:10:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021430#M15335</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-01-31T10:10:15Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021431#M15336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCU does not reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the MCU runs SPI read function, but data read is incorrect. This observation occurs with Rev D board only&lt;/P&gt;&lt;P&gt;but the same code works fine with Rev B board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Sanjib&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2020 05:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021431#M15336</guid>
      <dc:creator>sanjib_das</dc:creator>
      <dc:date>2020-02-03T05:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: SPI interface issue with MPC5748G Devkit Revision D</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021432#M15337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so external loopback is functional. With memory connected you can see all frames on the SPI bus, but the received data on MCU side is wrong, only fist word is correct.&lt;/P&gt;&lt;P&gt;This could lead to wrong timing or similar? Are you able to share some scope/analyzer screens where SPI frames are visible. Are they same between board revisions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 12:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPI-interface-issue-with-MPC5748G-Devkit-Revision-D/m-p/1021432#M15337</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-02-07T12:46:09Z</dc:date>
    </item>
  </channel>
</rss>