<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックS32DS Debugger view Variables doesn't work?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/S32DS-Debugger-view-Variables-doesn-t-work/m-p/992637#M14940</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear People,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a trivial problem: In the S32DS for Power Architecture, perspective&lt;BR /&gt;Debug, view Variables, I only see or get the local variables. I couldn't&lt;BR /&gt;find any way to add global variables to the list of displayed variables.&lt;BR /&gt;There are find operations, but they simply offer nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I doing something wrong? Do I misunderstand this view? Or is it a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This effect has been seen with versions 2017 R1 and 2.1. It's the same for&lt;BR /&gt;my own makefile projects and for sample projects I let the wizard create.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fortunately, it's not catastrophic since the other view Expressions works&lt;BR /&gt;fine. It offers even more functionality. The only drawback I found is that&lt;BR /&gt;the selection of variables is not so comfortable, one has to copy and paste&lt;BR /&gt;the name from the source code into a new expression instead of doing a&lt;BR /&gt;mouse click in a drop-down box as we know it from the well working view&lt;BR /&gt;variables in Code Warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I found out that view Expressions can be used to partly&lt;BR /&gt;circumvent a sad weakness of S32DS in comparison to Code Warrior: View&lt;BR /&gt;EmbSys Registers shows the I/O devices but doesn't show the SPRs of the&lt;BR /&gt;cores. In view Expression you can however enter everything, which we know&lt;BR /&gt;from the GDB client command line, particularly things like $SRR0 or $MCSR.&lt;BR /&gt;Still missing is CW's very handy display of bits and bit fields with short&lt;BR /&gt;explanation - even after years of work with PPC I don't know all MSR bits&lt;BR /&gt;by heart...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Nov 2019 16:01:58 GMT</pubDate>
    <dc:creator>peter_vranken</dc:creator>
    <dc:date>2019-11-29T16:01:58Z</dc:date>
    <item>
      <title>S32DS Debugger view Variables doesn't work?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32DS-Debugger-view-Variables-doesn-t-work/m-p/992637#M14940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear People,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a trivial problem: In the S32DS for Power Architecture, perspective&lt;BR /&gt;Debug, view Variables, I only see or get the local variables. I couldn't&lt;BR /&gt;find any way to add global variables to the list of displayed variables.&lt;BR /&gt;There are find operations, but they simply offer nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I doing something wrong? Do I misunderstand this view? Or is it a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This effect has been seen with versions 2017 R1 and 2.1. It's the same for&lt;BR /&gt;my own makefile projects and for sample projects I let the wizard create.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fortunately, it's not catastrophic since the other view Expressions works&lt;BR /&gt;fine. It offers even more functionality. The only drawback I found is that&lt;BR /&gt;the selection of variables is not so comfortable, one has to copy and paste&lt;BR /&gt;the name from the source code into a new expression instead of doing a&lt;BR /&gt;mouse click in a drop-down box as we know it from the well working view&lt;BR /&gt;variables in Code Warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I found out that view Expressions can be used to partly&lt;BR /&gt;circumvent a sad weakness of S32DS in comparison to Code Warrior: View&lt;BR /&gt;EmbSys Registers shows the I/O devices but doesn't show the SPRs of the&lt;BR /&gt;cores. In view Expression you can however enter everything, which we know&lt;BR /&gt;from the GDB client command line, particularly things like $SRR0 or $MCSR.&lt;BR /&gt;Still missing is CW's very handy display of bits and bit fields with short&lt;BR /&gt;explanation - even after years of work with PPC I don't know all MSR bits&lt;BR /&gt;by heart...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2019 16:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32DS-Debugger-view-Variables-doesn-t-work/m-p/992637#M14940</guid>
      <dc:creator>peter_vranken</dc:creator>
      <dc:date>2019-11-29T16:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Debugger view Variables doesn't work?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/S32DS-Debugger-view-Variables-doesn-t-work/m-p/992638#M14941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, for global variables the Expressions have to be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2019 10:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/S32DS-Debugger-view-Variables-doesn-t-work/m-p/992638#M14941</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-12-03T10:37:39Z</dc:date>
    </item>
  </channel>
</rss>