<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Loopback modes with TJA1100 Issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/978476#M14735</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In an Automotive project we are using TJA1100 as a PHY, I'm trying to validate the functionality of the 100BASE-T1 PCS and PMA functions.&lt;/P&gt;&lt;P&gt;So according to the TJA1100's datasheet in the loopback section,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100754i9651FF4311F7312A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I followed the steps to put the PHY in the external loopback mode as mentioned in the application notes AN12088&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100771i2A3375F45DD6F980/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But when I put the PHY in the external loopback I sent the data successfully but I didn't receive anything&lt;/P&gt;&lt;P&gt;To validate the loopback at all I tried the internal loopback mode, it works fine as Tx and Rx but also there was an issue which is the data transmitted on the bus, while it must not&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any answer please&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ahmed Saber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 21:19:31 GMT</pubDate>
    <dc:creator>ahmedsaber</dc:creator>
    <dc:date>2020-02-17T21:19:31Z</dc:date>
    <item>
      <title>Loopback modes with TJA1100 Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/978476#M14735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In an Automotive project we are using TJA1100 as a PHY, I'm trying to validate the functionality of the 100BASE-T1 PCS and PMA functions.&lt;/P&gt;&lt;P&gt;So according to the TJA1100's datasheet in the loopback section,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100754i9651FF4311F7312A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I followed the steps to put the PHY in the external loopback mode as mentioned in the application notes AN12088&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100771i2A3375F45DD6F980/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But when I put the PHY in the external loopback I sent the data successfully but I didn't receive anything&lt;/P&gt;&lt;P&gt;To validate the loopback at all I tried the internal loopback mode, it works fine as Tx and Rx but also there was an issue which is the data transmitted on the bus, while it must not&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any answer please&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ahmed Saber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 21:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/978476#M14735</guid>
      <dc:creator>ahmedsaber</dc:creator>
      <dc:date>2020-02-17T21:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: Loopback modes with TJA1100 Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/978477#M14736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you describe how you run external loopback test step by step?&lt;BR /&gt;What is TRX pins connection during the test?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 11:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/978477#M14736</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-02-18T11:43:42Z</dc:date>
    </item>
    <item>
      <title>Re: Loopback modes with TJA1100 Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1159145#M16554</link>
      <description>&lt;P&gt;hello ，can you tell me what's the problem you meet? how to solve this problem??&lt;/P&gt;&lt;P&gt;i meet the same problem like you.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 07:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1159145#M16554</guid>
      <dc:creator>misonyo</dc:creator>
      <dc:date>2020-09-25T07:15:48Z</dc:date>
    </item>
    <item>
      <title>Re: Loopback modes with TJA1100 Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1159673#M16556</link>
      <description>&lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt;&lt;P&gt;hello，should I connect TRX PINS to other PHYs?&amp;nbsp; I meet the same problem when i use TJA1101.&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2020 06:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1159673#M16556</guid>
      <dc:creator>misonyo</dc:creator>
      <dc:date>2020-09-27T06:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: Loopback modes with TJA1100 Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1306092#M18654</link>
      <description>&lt;P&gt;Hello Ahmed,&lt;/P&gt;&lt;P&gt;did you have any luck on this?&lt;/P&gt;&lt;P&gt;By the way, how did you manage to do even the internal loopback? So far I have had no success with that.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jul 2021 10:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Loopback-modes-with-TJA1100-Issue/m-p/1306092#M18654</guid>
      <dc:creator>thosewhowish2b</dc:creator>
      <dc:date>2021-07-12T10:10:14Z</dc:date>
    </item>
  </channel>
</rss>