<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5748G CAN-FD Reception in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977561#M14716</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RXIMRs are not accessible outside Freeze mode, so maybe debugger shows address value. When you put back to Freeze mode you should see right value again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 11:14:40 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-03-19T11:14:40Z</dc:date>
    <item>
      <title>MPC5748G CAN-FD Reception</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977558#M14713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Micontroller: MPC5748G&lt;/P&gt;&lt;P&gt;Peripheral: FlexCAN&lt;/P&gt;&lt;P&gt;Channel: CAN 0&lt;/P&gt;&lt;P&gt;Baudrate:&amp;nbsp;CAN-FD 1000 Kbps&lt;/P&gt;&lt;P&gt;Hardware: DevKit&lt;/P&gt;&lt;P&gt;Software: attached&lt;/P&gt;&lt;P&gt;Question: We are trying to Transmit a message on MB-0 and do an internal loop back to receive it back on MB-1. We do not see the message being received on the MB. Not sure if we are missing anything. Can we get some help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2020 13:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977558#M14713</guid>
      <dc:creator>bindu_madhavan</dc:creator>
      <dc:date>2020-03-17T13:23:07Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN-FD Reception</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977559#M14714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the header file does not distinguish memory partitions for CAN FD and it assumes just 8byte payload.&lt;/P&gt;&lt;P&gt;So when you access MB[1].CS it actually writes/reads MB offset 0x90 and no the correct one 0xC8 which is CS work of MB1 if 64 payload is configured.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So address the correct memory, see&amp;nbsp;Table 43-16 of the RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 13:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977559#M14714</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-03-18T13:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN-FD Reception</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977560#M14715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Petr.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other concern I saw was regarding RXIMR register. I had written 0x1FFFFFFF to most of the RXIMR registers and I see it getting loaded. But after clearing FRZ &amp;amp; HALT bits in MCR and a wait until FRZACK, they surprisingly get reassigned to its memory map address values&lt;/P&gt;&lt;P&gt;RXIMR[0] = 0xFFEC0880&lt;/P&gt;&lt;P&gt;RXIMR[1] = 0xFFEC0884&lt;/P&gt;&lt;P&gt;RXIMR[2] = 0xFFEC0888&lt;/P&gt;&lt;P&gt;RXIMR[3] = 0xFFEC088C&lt;/P&gt;&lt;P&gt;etc.&lt;/P&gt;&lt;P&gt;Any idea why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 09:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977560#M14715</guid>
      <dc:creator>bindu_madhavan</dc:creator>
      <dc:date>2020-03-19T09:21:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN-FD Reception</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977561#M14716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RXIMRs are not accessible outside Freeze mode, so maybe debugger shows address value. When you put back to Freeze mode you should see right value again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 11:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD-Reception/m-p/977561#M14716</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-03-19T11:14:40Z</dc:date>
    </item>
  </channel>
</rss>