<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mpc5748g debug problem in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972702#M14681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which LINFlex module is used? LINFlex_2? This one is connected to OpenSDA interface which works also as virtual serial port via USB. You wrote that you use Xchipi-X serial to usb adapter, so there may be a conflict between these signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 06:21:57 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2019-08-29T06:21:57Z</dc:date>
    <item>
      <title>mpc5748g debug problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972701#M14680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to run the code from :&lt;A class="link-bare" href="https://github.com/nanamiwang/openpilot/tree/flexray_bounty/flexray_adapter" title="https://github.com/nanamiwang/openpilot/tree/flexray_bounty/flexray_adapter"&gt;https://github.com/nanamiwang/openpilot/tree/flexray_bounty/flexray_adapter&lt;/A&gt;&amp;nbsp; on my&amp;nbsp;&lt;/P&gt;&lt;P&gt;mpc5748g, and when i try to use the debugger with putty or terterm as mentioned, i only get unreadable characters(attached picture), the baudrate seems to be right, i have tried to with other values also just in case but it didnt work.&lt;/P&gt;&lt;P&gt;I am using a Xchipi-X serial to usb adapter with a null modem adapter&lt;/P&gt;&lt;P&gt;i don't know what the problem is and i would appreciate any help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 15:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972701#M14680</guid>
      <dc:creator>omar_zayed</dc:creator>
      <dc:date>2019-08-26T15:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5748g debug problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972702#M14681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which LINFlex module is used? LINFlex_2? This one is connected to OpenSDA interface which works also as virtual serial port via USB. You wrote that you use Xchipi-X serial to usb adapter, so there may be a conflict between these signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 06:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972702#M14681</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-08-29T06:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5748g debug problem</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972703#M14682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your answer, in the code LINFLEX_4 was used with pins PA5 and PA6, but this didn't work, I have tried to use the LINFLEX_2 with OpenSDA interface and it worked, so i might guess that the problem is with the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Xchipi-X serial to usb adapter.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 07:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5748g-debug-problem/m-p/972703#M14682</guid>
      <dc:creator>omar_zayed</dc:creator>
      <dc:date>2019-09-03T07:50:37Z</dc:date>
    </item>
  </channel>
</rss>