<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックGPIO Clock</title>
    <link>https://community.nxp.com/t5/MPC5xxx/GPIO-Clock/m-p/953590#M14355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now I'm doing a custom GPIO/SIUL2 driver for the MPC5748G and I wanted to ask if there´s a way to set or gate off the clock for the GPIO pins or Port, for what I´ve seen now is that I´m able to use the GPIO ports and the SIUL2 even without configuring their clock using the clock driver.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My idea is if possible to be able to only enable to clock to a port or the GPIO if any of the pins are initialized. So Ill need to do that on my GPIO Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Aug 2019 16:27:19 GMT</pubDate>
    <dc:creator>ailtonlopes</dc:creator>
    <dc:date>2019-08-21T16:27:19Z</dc:date>
    <item>
      <title>GPIO Clock</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO-Clock/m-p/953590#M14355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now I'm doing a custom GPIO/SIUL2 driver for the MPC5748G and I wanted to ask if there´s a way to set or gate off the clock for the GPIO pins or Port, for what I´ve seen now is that I´m able to use the GPIO ports and the SIUL2 even without configuring their clock using the clock driver.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My idea is if possible to be able to only enable to clock to a port or the GPIO if any of the pins are initialized. So Ill need to do that on my GPIO Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 16:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO-Clock/m-p/953590#M14355</guid>
      <dc:creator>ailtonlopes</dc:creator>
      <dc:date>2019-08-21T16:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO Clock</title>
      <link>https://community.nxp.com/t5/MPC5xxx/GPIO-Clock/m-p/953591#M14356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;if there´s a way to set or gate off the clock for the GPIO pins or Port&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Yes, the SIUL belongs to Power domain 1 (PD1) which clock is gated off in Standby/LPU Standby mode.&lt;/P&gt;&lt;P&gt;Other than that SIUL don't have independent peripheral control bit in Mode entry module.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;My idea is if possible to be able to only enable to clock to a port or the GPIO if any of the pins are initialized. So Ill need to do that on my GPIO Driver.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Well, I understand. For this purpose you have DRUN mode which is active after reset and where all pins are configured as GPIO. After configuration is done you move to RUNx modes where the application runs and use the configured pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 07:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/GPIO-Clock/m-p/953591#M14356</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-08-22T07:14:48Z</dc:date>
    </item>
  </channel>
</rss>