<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5634M AUTOSAR OS example error</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949580#M14282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I escalated your question to automotive software team. They will contact you back directly by email.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jun 2019 10:29:23 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2019-06-06T10:29:23Z</dc:date>
    <item>
      <title>MPC5634M AUTOSAR OS example error</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949579#M14281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run AUTOSAR on MPC5634M with NXP MCAL&amp;amp;OS&amp;nbsp; with EB Tresos studio.&lt;/P&gt;&lt;P&gt;For this chip, NXP&amp;nbsp;supports AUTOSAR v 3.0.&lt;/P&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) I am using "Tresos Studio " Release ver 2009.a build number: b090820-1820.&lt;/P&gt;&lt;P&gt;OS Ver: Freescale AUTOSAR OS/MPC56xxAM v.3.0 RTM, build 3.0.35.&lt;/P&gt;&lt;P&gt;I have also added the patch "OSMPC56xxAM_3_0_35_patch1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I receive the following error (attached image) after importing the sample project: "os_sample_sc1" located in "\AUTOSAR\os_freescale_mpc56xxAM\os_ts\eclipse\workspace" to Tresos studio and running "Generate Project".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running on windows 7 64 bit system. Is a 32bit OS required for the configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)&amp;nbsp; The MCAL provided for the same chip is "AUTOSAR MPC563XM MCAL3.0 swv: 2.0.0 RTM". But this MCAL version expects "Tresos Studio ver 2010". But as stated in qn. 1), OS expects&amp;nbsp;&lt;SPAN&gt;"Tresos Studio " Release ver 2009.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;How&amp;nbsp; can i configure the entire project in this case, when there is a conflict in versions as seen here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help to&amp;nbsp;address the above questions and get the configurator to work is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your Sincerely,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Arjun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 12:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949579#M14281</guid>
      <dc:creator>arjunraveendran</dc:creator>
      <dc:date>2019-06-05T12:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5634M AUTOSAR OS example error</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949580#M14282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I escalated your question to automotive software team. They will contact you back directly by email.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2019 10:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949580#M14282</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2019-06-06T10:29:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5634M AUTOSAR OS example error</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949581#M14283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arjun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to the questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) I see the same error if generating on Windows 10 64-bit. The error is reported because by default on 64-bit operating system there is used 64-bit java. The MPC5634M Autosar OS supports only 32-bit java so to generate it is needed to install the 32-bit java. Then it is also needed to put the path to the 32-bit java to the PATH environmental variable so that it will be found while generating in Tresos.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The version of java can be checked with command java -version executed from command prompt:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;c:\&amp;gt;java -version&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;java version "1.8.0_201"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Java(TM) SE Runtime Environment (build 1.8.0_201-b09)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Java HotSpot(TM) 64-Bit Server VM (build 25.201-b09, mixed mode)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On my windows 10 computer there is used 64-bit java by default (see the string “64-Bit Server VM”).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have modified the path variable with the following command to add path to 32-bit java:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;c:\&amp;gt;path="c:\Program Files (x86)\Java\jre1.8.0_201\bin";%path%&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So then the java version reported is 32-bit (string “Client VM”) as shown here:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;c:\&amp;gt;java -version&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;java version "1.8.0_201"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Java(TM) SE Runtime Environment (build 1.8.0_201-b09)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Java HotSpot(TM) Client VM (build 25.201-b09, mixed mode)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this I open the Tresos with this command (still in the same command prompt window):&lt;/P&gt;&lt;P&gt;&lt;EM&gt;c:\&amp;gt;c:\EB\tresos2010.a.sr4\bin\tresos_gui.exe&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and I can generate correctly without any error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you prefer you can just add the path to the 32-bit java to your PATH environmental variable so that 32-bit java would be always used (but be careful that this could impact other programs that might require 64-bit java).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) There can be used the newer version (Tresos 2010.sr4) to configure both MCAL and OS. See the MCAL sample application (located in c:\Freescale\AUTOSAR\MPC563XM_MCAL3.0_RTM_2.0.0_signed\MPC563XM_MCAL3.0_RTM_2.0.0_Integration_Application) where both MCAL and OS are integrated within one project. See here the screenshot from Tresos:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88052iF0F2B93CCF1227DF/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Frantisek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 21:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949581#M14283</guid>
      <dc:creator>frantisekdobes</dc:creator>
      <dc:date>2019-06-17T21:48:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5634M AUTOSAR OS example error</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949582#M14284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frantisek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp; a lot for the solution.&lt;/P&gt;&lt;P&gt;It has worked perfectly well and now I am able to generate code from Tresos studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp; a lot for taking the time out to answer this query in detail.&lt;/P&gt;&lt;P&gt;Good day to you.&lt;/P&gt;&lt;P&gt;Arjun.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 09:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5634M-AUTOSAR-OS-example-error/m-p/949582#M14284</guid>
      <dc:creator>arjunraveendran</dc:creator>
      <dc:date>2019-06-19T09:56:36Z</dc:date>
    </item>
  </channel>
</rss>