<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the relationship between FMPLL and BIUCR? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926540#M13862</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are APC, WWSC and RWSC bit fields in the BIUCR which are used to configure flash wait states:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81833i8EE32350532588CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;And in the datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81873i0563F2C1C3DDA114/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;For 150MHz, there should be 0x----9C--&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can re-use initialization code from:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101455"&gt;https://community.nxp.com/docs/DOC-101455&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jul 2019 04:53:38 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2019-07-17T04:53:38Z</dc:date>
    <item>
      <title>What is the relationship between FMPLL and BIUCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926539#M13861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hello,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I'm using a&lt;SPAN style="border: 0px; font-weight: inherit;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;MPC5644A&lt;/STRONG&gt;&lt;SPAN style="border: 0px; font-weight: inherit;"&gt;&amp;nbsp;&lt;/SPAN&gt;and want to set the maximum value of the system frequency (150MHz). However,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;If the system frequency is set to values greater than 82MHz, I have to make the following definitions in the &lt;STRONG&gt;__ppc_eabi_init&lt;/STRONG&gt; file.&amp;nbsp;Why are these definitions made in &lt;STRONG&gt;__ppc_eabi_init&amp;nbsp;&lt;/STRONG&gt;file? What is the relationship between FMPLL and BIUCR?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80011iAD224177FBDE21C5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thank you for your help...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 20:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926539#M13861</guid>
      <dc:creator>tgc-yilmaz</dc:creator>
      <dc:date>2019-07-16T20:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: What is the relationship between FMPLL and BIUCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926540#M13862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are APC, WWSC and RWSC bit fields in the BIUCR which are used to configure flash wait states:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81833i8EE32350532588CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;And in the datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81873i0563F2C1C3DDA114/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;For 150MHz, there should be 0x----9C--&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can re-use initialization code from:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101455"&gt;https://community.nxp.com/docs/DOC-101455&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 04:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926540#M13862</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-07-17T04:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: What is the relationship between FMPLL and BIUCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926541#M13863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hello Lukas Zadrapa,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&amp;nbsp;I am asking for be sure. We do these definitions in order to be able to read properly from flash at higher operating frequencies. In this way, we prevent the error in the code by associating the flash reading speed with the operating frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 19:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926541#M13863</guid>
      <dc:creator>tgc-yilmaz</dc:creator>
      <dc:date>2019-07-17T19:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: What is the relationship between FMPLL and BIUCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926542#M13864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that's correct. The flash is not so fast, so if higher system clock is used, it's necessary to wait until the flash is able to provide requested data - this is managed by flash wait states. By default, the flash wait state are always configured to maximum. For best performance, it's necessary to follow the mentioned table from the datasheet and configure it appropriately. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 07:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/What-is-the-relationship-between-FMPLL-and-BIUCR/m-p/926542#M13864</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-07-18T07:23:37Z</dc:date>
    </item>
  </channel>
</rss>