<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5606B : EMIOS Module as GPIO</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447700#M1382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not give you a hint for the RAppID setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But generally, the pad itself should be programmed to eMIOS function&amp;nbsp; by PCR[PA] field in case of output and IBE bit for the input.&lt;/P&gt;&lt;P&gt;The eMIOS GPIO input /output mode is set by programming the MODE field of CCR register. &lt;/P&gt;&lt;P&gt;For GPIO input mode, the input pin status can be determined by reading the UCIN bit.&lt;/P&gt;&lt;P&gt;For GPIO output mode, the unified channel is used as a single output port pin and the value of the EDPOL bit is permanently transferred to the output flip-flop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Nov 2015 08:16:03 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2015-11-30T08:16:03Z</dc:date>
    <item>
      <title>MPC5606B : EMIOS Module as GPIO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447699#M1381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am little confused on the usage of EMIOS as GPIO.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use EMIOS 1 module as general purpose input/output and i want to configure it through RAPPID Tool. What are all the recommended settings to be done?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an input,&lt;/P&gt;&lt;P&gt;Which register of EMIOS should i check to read the input which is connected to the corresponding Emios port.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an output,&lt;/P&gt;&lt;P&gt;Which register of EMIOS should i use to trigger the output which is connected to the corresponding Emios port.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Raghavendra P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 11:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447699#M1381</guid>
      <dc:creator>raghavendrapura</dc:creator>
      <dc:date>2015-11-27T11:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B : EMIOS Module as GPIO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447700#M1382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not give you a hint for the RAppID setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But generally, the pad itself should be programmed to eMIOS function&amp;nbsp; by PCR[PA] field in case of output and IBE bit for the input.&lt;/P&gt;&lt;P&gt;The eMIOS GPIO input /output mode is set by programming the MODE field of CCR register. &lt;/P&gt;&lt;P&gt;For GPIO input mode, the input pin status can be determined by reading the UCIN bit.&lt;/P&gt;&lt;P&gt;For GPIO output mode, the unified channel is used as a single output port pin and the value of the EDPOL bit is permanently transferred to the output flip-flop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2015 08:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447700#M1382</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2015-11-30T08:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5606B : EMIOS Module as GPIO</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447701#M1383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Raghavendra Puranik ,Petr&lt;/P&gt;&lt;P&gt;now I am also working on gpio modes of emios for mpc5676r . can I know where we should go with gpio input mode and out put mode how this gpio modes differ from other modes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please Raghavendra Puranik can you have sample gpio I am trying I have not getting clearly .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 09:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5606B-EMIOS-Module-as-GPIO/m-p/447701#M1383</guid>
      <dc:creator>mpc5676r</dc:creator>
      <dc:date>2016-03-03T09:11:55Z</dc:date>
    </item>
  </channel>
</rss>