<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5643L create SRAM region uncacheable in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906293#M13486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lukaszadrapa"&gt;lukaszadrapa&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK, if I understand well we can combine several TLB of different size to make the desired granularity. In my case I need to set :&lt;/P&gt;&lt;P&gt;SRAM region Cacheable : 1 TLB of 64K + 1 TLB of 32K + 1 TLB of 16K + 1 TLB of 8K&lt;/P&gt;&lt;P&gt;SRAM region uncacheable : 1 TLB of 8K&lt;/P&gt;&lt;P&gt;That gives total of 128K SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2019 06:52:02 GMT</pubDate>
    <dc:creator>Pat</dc:creator>
    <dc:date>2019-04-24T06:52:02Z</dc:date>
    <item>
      <title>MPC5643L create SRAM region uncacheable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906291#M13484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Now, I have a MMU TLB entry definition for the SRAM as : TSIZE of 128K and cacheable.&lt;/P&gt;&lt;P&gt;I would like create a new region of i.e 2KB of SRAM uncacheable. So at the end, I would have 2 regions one of 126KB and the second of 2KB.&lt;/P&gt;&lt;P&gt;As my understanding, the MMU can't be used because the granularity (TSIZE 64K or 128K) is too big. So I need to use the MPU to create such region, right ? Or I'm totally wrong ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 12:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906291#M13484</guid>
      <dc:creator>Pat</dc:creator>
      <dc:date>2019-04-23T12:24:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L create SRAM region uncacheable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906292#M13485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;minimal size of MMU page is 1k in case of e200z4 core, so I can't see problem here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80732iE571A8D816EF09A7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;This excel configuration tool could help:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331924"&gt;MMU Assist Register CONFIGURATOR&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notice that all MMU pages must be aligned. For example, 2K page must be aligned to 2K boundary, 128K page must be aligned to 128K boundary. So, if you need to create 2K page, you will need more pages to cover rest of the area.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MPU can't be used to make some area cache inhibited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 06:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906292#M13485</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-04-24T06:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L create SRAM region uncacheable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906293#M13486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lukaszadrapa"&gt;lukaszadrapa&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OK, if I understand well we can combine several TLB of different size to make the desired granularity. In my case I need to set :&lt;/P&gt;&lt;P&gt;SRAM region Cacheable : 1 TLB of 64K + 1 TLB of 32K + 1 TLB of 16K + 1 TLB of 8K&lt;/P&gt;&lt;P&gt;SRAM region uncacheable : 1 TLB of 8K&lt;/P&gt;&lt;P&gt;That gives total of 128K SRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Pat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 06:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906293#M13486</guid>
      <dc:creator>Pat</dc:creator>
      <dc:date>2019-04-24T06:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643L create SRAM region uncacheable</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906294#M13487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that's it, your understanding is correct. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 06:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5643L-create-SRAM-region-uncacheable/m-p/906294#M13487</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-04-24T06:56:52Z</dc:date>
    </item>
  </channel>
</rss>