<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5748G CAN FD</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902285#M13372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there should not be an issue to make communication between those boards. You should keep following...&lt;/P&gt;&lt;P&gt;- use 12V power supply to power both boards to enable SBC's CAN transceiver&lt;/P&gt;&lt;P&gt;- boards are connected using 3 wires (CANH, CANL, GND)&lt;/P&gt;&lt;P&gt;-&amp;nbsp;DEVKIT_MCP5748G&amp;nbsp;does not have termination resistor, so it could be needed in case of communication issues&lt;/P&gt;&lt;P&gt;- the same bitrate including sample point must be set on both MCUs&lt;/P&gt;&lt;P&gt;- check if both MCU use the same CAN FD protocol, is configurable by CTRL2[ISOCANFDEN] bit&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Apr 2019 07:46:52 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-04-25T07:46:52Z</dc:date>
    <item>
      <title>MPC5748G CAN FD</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902282#M13369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all , I want to use the communication CAN FD on MPC5748G. I look some information with NXP Community. I find out some example but all of them can not work. So who can help me to bring up CAN FD module on MPC5748G.&amp;nbsp;&lt;BR /&gt;Thank you.&lt;BR /&gt;I try to following some example I attach bellow, but it can not work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 07:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902282#M13369</guid>
      <dc:creator>nguyencongtruon</dc:creator>
      <dc:date>2019-04-19T07:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN FD</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902283#M13370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you use EVBs for test or do you have your own board design? What is the bus connection, who is the other node?&lt;/P&gt;&lt;P&gt;The examples you pointed do communication between modules on the EVB, i realized it does not set FD timing properly.&lt;/P&gt;&lt;P&gt;So it can work on the EVB but it could not work between boards and/or PC etc.&lt;/P&gt;&lt;P&gt;What is not working in fact? You cannot send/receive anything? Do you get any errors?&lt;/P&gt;&lt;P&gt;I can suggest to review the CAN bit timing setting, you can use a tool posted here (&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-342618"&gt;https://community.nxp.com/docs/DOC-342618&lt;/A&gt;) to get right setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 08:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902283#M13370</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-04-23T08:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN FD</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902284#M13371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your support.&amp;nbsp;&lt;BR /&gt;I'm using DEVKIT_MCP5748G to communication with S43K144-EVB board via CAN_FD. Follow you suggest in order to communicate between 2 board,&amp;nbsp; do I just need to change the bit timing configure to communicate between 2 board?&amp;nbsp;I'll try to change the configuration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;TruongN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 07:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902284#M13371</guid>
      <dc:creator>nguyencongtruon</dc:creator>
      <dc:date>2019-04-24T07:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5748G CAN FD</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902285#M13372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there should not be an issue to make communication between those boards. You should keep following...&lt;/P&gt;&lt;P&gt;- use 12V power supply to power both boards to enable SBC's CAN transceiver&lt;/P&gt;&lt;P&gt;- boards are connected using 3 wires (CANH, CANL, GND)&lt;/P&gt;&lt;P&gt;-&amp;nbsp;DEVKIT_MCP5748G&amp;nbsp;does not have termination resistor, so it could be needed in case of communication issues&lt;/P&gt;&lt;P&gt;- the same bitrate including sample point must be set on both MCUs&lt;/P&gt;&lt;P&gt;- check if both MCU use the same CAN FD protocol, is configurable by CTRL2[ISOCANFDEN] bit&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2019 07:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5748G-CAN-FD/m-p/902285#M13372</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-04-25T07:46:52Z</dc:date>
    </item>
  </channel>
</rss>