<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VSTBY in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893534#M13205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok,thanks very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 May 2019 09:20:37 GMT</pubDate>
    <dc:creator>pwok2004</dc:creator>
    <dc:date>2019-05-20T09:20:37Z</dc:date>
    <item>
      <title>VSTBY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893530#M13201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing the hardware circuit of spc5644A.&lt;BR /&gt;SRAM standby functionality is required, but I do not know how to handle VSTBY pins.&lt;BR /&gt;I don't know if I need an external power supply or not.&lt;/P&gt;&lt;P&gt;now, only an external RC circuit is connected to the processing, and there is no power supply.&lt;BR /&gt;I don't know if it's right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81154i96FE5C6B3861CFAD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 03:42:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893530#M13201</guid>
      <dc:creator>pwok2004</dc:creator>
      <dc:date>2019-05-15T03:42:06Z</dc:date>
    </item>
    <item>
      <title>Re: VSTBY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893531#M13202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, SRAM can be backed up directly by 1V power rail or “indirectly” from 2-5.5V when standby regulator derives 1V from that automatically. It removes the need of separate 1V rail. 1-2V and 0.2V-0.95V voltage are forbidden areas.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When&lt;/P&gt;&lt;P&gt;VSTBY = 0-0.2V then standby function is disabled completely&lt;/P&gt;&lt;P&gt;VSTBY = 0.95-1.2V then standby regulator is disabled and standby RAM is fed directly&lt;/P&gt;&lt;P&gt;VSTBY = 2-5.5V then standby regulator is enabled and standby RAM is fed by 1V output of this regulator (internally).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess the screenshot is wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 08:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893531#M13202</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-05-15T08:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: VSTBY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893532#M13203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Thanks for your reply.&lt;/P&gt;&lt;P&gt;Does whether &amp;nbsp;it&amp;nbsp;mean that &amp;nbsp;in my circuit, I need to connect the external power supply of 2-2.5v to the VSTBY pin?&lt;/P&gt;&lt;P&gt;As shown in the figure below:&lt;/P&gt;&lt;P&gt;thanks very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81397i44B695EEED644635/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 May 2019 00:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893532#M13203</guid>
      <dc:creator>pwok2004</dc:creator>
      <dc:date>2019-05-17T00:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: VSTBY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893533#M13204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not 2-2.5V but 2-5.5V, typically 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See AN4291, section 3.3:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4291.pdf" title="https://www.nxp.com/docs/en/application-note/AN4291.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4291.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 May 2019 05:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893533#M13204</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-05-17T05:11:10Z</dc:date>
    </item>
    <item>
      <title>Re: VSTBY</title>
      <link>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893534#M13205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok,thanks very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 09:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/VSTBY/m-p/893534#M13205</guid>
      <dc:creator>pwok2004</dc:creator>
      <dc:date>2019-05-20T09:20:37Z</dc:date>
    </item>
  </channel>
</rss>