<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877915#M12904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have an example code for the device's predecessor MPC5676R:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335461"&gt;https://community.nxp.com/docs/DOC-335461&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2019 13:53:05 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2019-02-20T13:53:05Z</dc:date>
    <item>
      <title>Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877914#M12903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I need to read and write and flash 128MB &lt;SPAN style="color: #000000; font-size: 12px;"&gt;FLASH - NOR (&lt;/SPAN&gt;cypress semiconductor) flash from mpc5777c using DSPI&amp;nbsp; (DSPI_C) . How to start with it any application note or example present for the same. kindly guide me through.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 11:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877914#M12903</guid>
      <dc:creator>vignesh_v</dc:creator>
      <dc:date>2019-02-20T11:02:27Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877915#M12904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have an example code for the device's predecessor MPC5676R:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335461"&gt;https://community.nxp.com/docs/DOC-335461&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 13:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877915#M12904</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-02-20T13:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877916#M12905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks but can the framework used for mpc5777c or it is vastly different from each other.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 14:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877916#M12905</guid>
      <dc:creator>vignesh_v</dc:creator>
      <dc:date>2019-02-20T14:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877917#M12906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here you may find some example codes for MPC5777C as well.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329623"&gt;https://community.nxp.com/docs/DOC-329623&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DSPI module itself is the same so it should not be difficult combine it together.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 15:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877917#M12906</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-02-20T15:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877918#M12907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help. One Query,&lt;/P&gt;&lt;P&gt;In the example the READ ID command is used (0X90)&amp;nbsp; to read manufacture ID and device ID&lt;/P&gt;&lt;P&gt;If it has to be read with 0x9F command how to proceed with it can u kindly help.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks In Advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 05:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877918#M12907</guid>
      <dc:creator>vignesh_v</dc:creator>
      <dc:date>2019-02-26T05:35:07Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877919#M12908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A file dspi_S25FL129.h contains commands for SPI memory S25FL129. Please edit it or create your own file for the memory you are using. Command set you should find in the datasheet of specific external memory.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 08:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877919#M12908</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-02-26T08:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding accessing external flash  from MPC5777c using DSPI</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877920#M12909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks. I got what u said but what i wanted to ask the memory i use is very similar to one used..if u could explain how to use it for read instruction 0x9F&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="border: 0px; font-weight: inherit;"&gt;&amp;nbsp;&lt;/SPAN&gt;for SPI memory S25FL129 it would be helpful for me to get a an idea for the same. I'm slightly in doubt how to read one byte of manufacture followed by 2 bytes of device id. if u could explain the same for memory thats been used in the example it would be helpful.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN&gt;Thanks In Advance.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 05:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Regarding-accessing-external-flash-from-MPC5777c-using-DSPI/m-p/877920#M12909</guid>
      <dc:creator>vignesh_v</dc:creator>
      <dc:date>2019-03-07T05:53:45Z</dc:date>
    </item>
  </channel>
</rss>