<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Lockstep and dual couple modes in MPC5746R Microcontroller  in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866482#M12752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please provide information about the MPC546R cores operation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2019 07:38:52 GMT</pubDate>
    <dc:creator>damu_nagarimadu</dc:creator>
    <dc:date>2019-02-15T07:38:52Z</dc:date>
    <item>
      <title>Lockstep and dual couple modes in MPC5746R Microcontroller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866482#M12752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please provide information about the MPC546R cores operation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 07:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866482#M12752</guid>
      <dc:creator>damu_nagarimadu</dc:creator>
      <dc:date>2019-02-15T07:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: Lockstep and dual couple modes in MPC5746R Microcontroller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866483#M12753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, MPC57xx does not use LSM/DPM modes, but device has main core and checker core (so called Safety Lake) as you can see in the picture below. These can be enabled or disabled, thus the protection is available or not, but safety lakes cannot be used for increasing of device overall performance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Main core and checker are almost the same, but differs in absence of some sub-blocks in its checker variant (caches, nexus). Its number is decreased by one (e200z720 -&amp;gt; e200z719). Safety core operates in delayed lockstep mode (LSM) to allow the &lt;SPAN style="font-size: 12.0pt;"&gt;highest safety level to be reached. The checker core will receive all inputs delayed by two clock cycles. Outputs of the checker core will be compared with outputs of the master core. Any differences will be flagged as an error and processed by the FCCU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72311iB3BC9585638330B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps to understand the principle.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 19:05:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866483#M12753</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-02-15T19:05:35Z</dc:date>
    </item>
    <item>
      <title>Re: Lockstep and dual couple modes in MPC5746R Microcontroller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866484#M12754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;Thanks for quick update on Core operations. I am planning to run the two cores with deferent software's and I need to enable safety lake as well. So could you please provide sample code to run the two different SW on the two main cores and safety lake enable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Damu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 06:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866484#M12754</guid>
      <dc:creator>damu_nagarimadu</dc:creator>
      <dc:date>2019-02-18T06:32:30Z</dc:date>
    </item>
    <item>
      <title>Re: Lockstep and dual couple modes in MPC5746R Microcontroller</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866485#M12755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Such example you may find for instance here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332669"&gt;Example MPC5746R DPM (multicore) GHS614&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the difference telling whether safety lake is enabled or not is LOCKSTEP EN bit in the DCF_UTEST_Miscellaneous client. By default lockstep in enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means in the moment Main Core 0 is enabled, Checker Core 0s is enabled as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 12:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Lockstep-and-dual-couple-modes-in-MPC5746R-Microcontroller/m-p/866485#M12755</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-02-18T12:20:01Z</dc:date>
    </item>
  </channel>
</rss>