<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPC5606BF1MLQ6 CAN1 Low Power Issue in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/SPC5606BF1MLQ6-CAN1-Low-Power-Issue/m-p/847065#M12434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I built the project which used CAN1module, I need to let CAN1 go to low power model, that I set the TX, RX port to GPIO model. However, I found when set CAN1 to GPIO, then delay some millisecond, after that set CAN1 to Freese/Disable model, go to sleep, the current can low to 3mA. And, if set CAN1 to GPIO, set CAN1 to Freese/Disable model, delay some milesecond, then sleep, the current reach to 26mA. I found the RX_ERROR_COUNTER cannot be cleared, it is 129.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Can anybody help to advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray Deng&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jul 2018 13:41:01 GMT</pubDate>
    <dc:creator>dannydeng</dc:creator>
    <dc:date>2018-07-04T13:41:01Z</dc:date>
    <item>
      <title>SPC5606BF1MLQ6 CAN1 Low Power Issue</title>
      <link>https://community.nxp.com/t5/MPC5xxx/SPC5606BF1MLQ6-CAN1-Low-Power-Issue/m-p/847065#M12434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I built the project which used CAN1module, I need to let CAN1 go to low power model, that I set the TX, RX port to GPIO model. However, I found when set CAN1 to GPIO, then delay some millisecond, after that set CAN1 to Freese/Disable model, go to sleep, the current can low to 3mA. And, if set CAN1 to GPIO, set CAN1 to Freese/Disable model, delay some milesecond, then sleep, the current reach to 26mA. I found the RX_ERROR_COUNTER cannot be cleared, it is 129.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Can anybody help to advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ray Deng&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 13:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/SPC5606BF1MLQ6-CAN1-Low-Power-Issue/m-p/847065#M12434</guid>
      <dc:creator>dannydeng</dc:creator>
      <dc:date>2018-07-04T13:41:01Z</dc:date>
    </item>
  </channel>
</rss>