<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Erase/Program Disturb Limits for MPC5777C Flash Memory in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Erase-Program-Disturb-Limits-for-MPC5777C-Flash-Memory/m-p/834088#M12259</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a query related to MPC5777C Controller - FLASH Memory.&lt;/P&gt;&lt;P&gt;The datasheet does mention about the Number of program/erase cycles per block &amp;amp; data retention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I want to confirm if there are any erase/program disturb limits also? Will they vary as per temperature ranges?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Disturb limits for Flash : This is the limit to study the robustness of the data storage of the flash cells when the state of a nearby cell is being changed, either through erasing, programming or reading. A disturb failure means that the initial state of the cell has been changed to the opposite state as result of erasing, programming or reading.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2018 09:41:04 GMT</pubDate>
    <dc:creator>charukamboj</dc:creator>
    <dc:date>2018-10-25T09:41:04Z</dc:date>
    <item>
      <title>Erase/Program Disturb Limits for MPC5777C Flash Memory</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Erase-Program-Disturb-Limits-for-MPC5777C-Flash-Memory/m-p/834088#M12259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a query related to MPC5777C Controller - FLASH Memory.&lt;/P&gt;&lt;P&gt;The datasheet does mention about the Number of program/erase cycles per block &amp;amp; data retention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I want to confirm if there are any erase/program disturb limits also? Will they vary as per temperature ranges?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Disturb limits for Flash : This is the limit to study the robustness of the data storage of the flash cells when the state of a nearby cell is being changed, either through erasing, programming or reading. A disturb failure means that the initial state of the cell has been changed to the opposite state as result of erasing, programming or reading.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 09:41:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Erase-Program-Disturb-Limits-for-MPC5777C-Flash-Memory/m-p/834088#M12259</guid>
      <dc:creator>charukamboj</dc:creator>
      <dc:date>2018-10-25T09:41:04Z</dc:date>
    </item>
    <item>
      <title>Re: Erase/Program Disturb Limits for MPC5777C Flash Memory</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Erase-Program-Disturb-Limits-for-MPC5777C-Flash-Memory/m-p/834089#M12260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;But I want to confirm if there are any erase/program disturb limits also? Will they vary as per temperature ranges?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;There are no limits except Number of program/erase cycles per block &amp;amp; data retention in datasheet.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;regards,&lt;BR /&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 08:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Erase-Program-Disturb-Limits-for-MPC5777C-Flash-Memory/m-p/834089#M12260</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-04-17T08:37:38Z</dc:date>
    </item>
  </channel>
</rss>