<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックCTU_0 and CTU_1 same trigger source</title>
    <link>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824694#M12136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way to trigger CTU_0 and CTU_1 from FlexPWM_1 only?. if not how this is possible to achieve as I want to sample ADC0,1 and 2 at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ali&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 08:15:25 GMT</pubDate>
    <dc:creator>alimeraj</dc:creator>
    <dc:date>2018-07-18T08:15:25Z</dc:date>
    <item>
      <title>CTU_0 and CTU_1 same trigger source</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824694#M12136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way to trigger CTU_0 and CTU_1 from FlexPWM_1 only?. if not how this is possible to achieve as I want to sample ADC0,1 and 2 at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ali&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 08:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824694#M12136</guid>
      <dc:creator>alimeraj</dc:creator>
      <dc:date>2018-07-18T08:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: CTU_0 and CTU_1 same trigger source</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824695#M12137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you need to trigger CTU0 and1 from your PWM signal.&lt;/P&gt;&lt;P&gt;Then you will have in CTU0 command list dual conversion for ADC0 and 1.&lt;/P&gt;&lt;P&gt;In CTU1 command list you will have ADC2.&lt;/P&gt;&lt;P&gt;Make sure CTUs triggers are executed in the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 08:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824695#M12137</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2018-07-18T08:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: CTU_0 and CTU_1 same trigger source</title>
      <link>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824696#M12138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for coming back to my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem here is I am only using flexPWM_1 module to generate PWM and I can trigger ADC2 using CTU1 properly. the only issue I have is how can trigger the CTU0 from flexPWM_1 module or if there is any other way to sample ADC0 and ADC1 at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ali&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 09:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/CTU-0-and-CTU-1-same-trigger-source/m-p/824696#M12138</guid>
      <dc:creator>alimeraj</dc:creator>
      <dc:date>2018-07-18T09:05:26Z</dc:date>
    </item>
  </channel>
</rss>