<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash a release build using OpenSDA in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Flash-a-release-build-using-OpenSDA/m-p/795535#M11611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a project using S32DS for MPC5748G. During development, I used to build the project in debug mode and use OpenSDA for flashing the code to MPC. The same is used for debug purpose as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want to flash the binary generated in release mode. Can I use the OpenSDA for the same? What changes are required for this to use OpenSDA for flashing the binary to MPC target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without using S32DS, how can I flash my code to MPC target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Oct 2018 05:53:57 GMT</pubDate>
    <dc:creator>sk4</dc:creator>
    <dc:date>2018-10-16T05:53:57Z</dc:date>
    <item>
      <title>Flash a release build using OpenSDA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-a-release-build-using-OpenSDA/m-p/795535#M11611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a project using S32DS for MPC5748G. During development, I used to build the project in debug mode and use OpenSDA for flashing the code to MPC. The same is used for debug purpose as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want to flash the binary generated in release mode. Can I use the OpenSDA for the same? What changes are required for this to use OpenSDA for flashing the binary to MPC target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without using S32DS, how can I flash my code to MPC target?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 05:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-a-release-build-using-OpenSDA/m-p/795535#M11611</guid>
      <dc:creator>sk4</dc:creator>
      <dc:date>2018-10-16T05:53:57Z</dc:date>
    </item>
    <item>
      <title>Re: Flash a release build using OpenSDA</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Flash-a-release-build-using-OpenSDA/m-p/795536#M11612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;yes you can use it, here is the example:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342465"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Without using S32DS, how can I flash my code to MPC target?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;You can use any debugger interface which supports MPC57xx devices with JTAG:&lt;/P&gt;&lt;P&gt;For example PEMicro, Lauterbach, iSystem, PLS, GHS, etc...&lt;/P&gt;&lt;P&gt;Each of this has different steps for loading the code into micro.&lt;/P&gt;&lt;P&gt;or you can use serial boot mode via serial communication interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;BR /&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2019 12:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Flash-a-release-build-using-OpenSDA/m-p/795536#M11612</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-02-25T12:55:03Z</dc:date>
    </item>
  </channel>
</rss>