<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790627#M11547</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;And what you really want to do?&lt;/P&gt;&lt;P&gt;1. Insert a real fault into BIST testing&lt;/P&gt;&lt;P&gt;2. Just to test reaction on faulty BIST results&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;If the CPU detects a fault during the off-line BIST it will stay in reset and after 8 seconds the SBC will enter Deep fail safe state (the system is powered off), correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The CPU is not capable of detecting fault during off-line BIST. I works on MISR patterns. So, after BIST is finished, there is result output in MISR which is compared with expected MISR provided by NXP.&lt;/P&gt;&lt;P&gt;The BIST reports faults after it is finished with testing and comparing the MISR results. This is no issue as BIST is running during RESET and this is considered as safe state. No application is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 05:58:21 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2018-08-16T05:58:21Z</dc:date>
    <item>
      <title>Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790626#M11546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/petervlna"&gt;petervlna&lt;/A&gt;‌&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Hello Mr Vlna,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Please refer our discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-334419"&gt;Using the Built-in Self-Test (BIST) on the MPC5744P&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;We are using the MPC5744P CPU together with the System Basis Chip (SBC) 33907.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;We are considering how to test the BIST functionality. As you mention one&amp;nbsp;method would be to start the system with a low power supply level. But, what will actually happen is that the SBC will detect the low power and hold the CPU in reset?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Do you see any other methods to verify the CPU BIST?&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;If the CPU detects a fault during the off-line BIST it will stay in reset and after 8 seconds the SBC will enter Deep fail safe state (the system is powered off), correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Peder&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 07:30:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790626#M11546</guid>
      <dc:creator>pederrogo</dc:creator>
      <dc:date>2018-08-15T07:30:38Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790627#M11547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;And what you really want to do?&lt;/P&gt;&lt;P&gt;1. Insert a real fault into BIST testing&lt;/P&gt;&lt;P&gt;2. Just to test reaction on faulty BIST results&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;If the CPU detects a fault during the off-line BIST it will stay in reset and after 8 seconds the SBC will enter Deep fail safe state (the system is powered off), correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The CPU is not capable of detecting fault during off-line BIST. I works on MISR patterns. So, after BIST is finished, there is result output in MISR which is compared with expected MISR provided by NXP.&lt;/P&gt;&lt;P&gt;The BIST reports faults after it is finished with testing and comparing the MISR results. This is no issue as BIST is running during RESET and this is considered as safe state. No application is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 05:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790627#M11547</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2018-08-16T05:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790628#M11548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;What we really want to verify is:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt; That the off-line BIST is enabled and can detect any faults.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt; That the reaction on any fault is as expected, i.e. the CPU stays in reset and that the SBC eventually sets the ECU in Deep fail safe (power off).&amp;nbsp;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Maybe one method to verify 1 could be to read out the BIST result registers you mention in the Application Note &lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&lt;A href="https://community.nxp.com/legacyfs/online/275452_MPC5744P_STCU2_BIST_v0_3.pdf"&gt;&lt;STRONG style="border: none windowtext 1.0pt; padding: 0cm; color: #3d9ce7; font-size: 9.0pt;"&gt;MPC5744P_STCU2_BIST_v0_3.pdf:&amp;nbsp;&lt;/STRONG&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;STCU2_ERR_STAT&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;STCU2_LBS&lt;BR /&gt; STCU2_LBE&lt;BR /&gt; STCU2_MBSL&lt;BR /&gt; STCU2_MBEL&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;I.e. if these registers show that the tests are completed successfully it could be assumed that the off-line BIST is enabled. But, to verify 2 we assume a fault has to be injected somehow...&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Peder&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 06:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790628#M11548</guid>
      <dc:creator>pederrogo</dc:creator>
      <dc:date>2018-08-16T06:32:22Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790629#M11549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. If BIST is enabled or not is signalized by BYP bit&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63116iA9FCF630932F702B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63149i8790D0F040E3B013/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You won't find this description in MPC5744P reference manual as NXP decided not to give configuration choice for MPC5744P users. But if you are interested in STCU register content you can see it in MPC5746R reference manual for example. Module is the same but number of tested partitions differs from micro to micro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simply enabled BIST desnt't means that it will check the device. You have to see if the STCU2_CFG pointer is set on first desired test. In this case 0x12. Because if the pointer is 0x7F then BIST is bypassed also.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63221i9DF7336FC5077D1C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63249i06E66D035D011F2F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So check:&lt;/P&gt;&lt;P&gt;1. BYP bit&lt;/P&gt;&lt;P&gt;2. pointer (PTR)&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;To check the reaction you can fake the MISR results.&lt;/P&gt;&lt;P&gt;For example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63290iE47D8E35300C8B19/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Program to MISR different values then you can see in upper table. Then the BIST will report errors in ERR_STAT register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 07:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790629#M11549</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2018-08-16T07:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790630#M11550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Peter,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Thanks for your quick response. The first part above reg checking if BIST is enable or not seems quite straight forward. But, how would actually the sequence be in order to inject a fault that BIST detects? It includes on-line BIST and a sequence according the Application Note (&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&lt;A href="https://community.nxp.com/legacyfs/online/275452_MPC5744P_STCU2_BIST_v0_3.pdf"&gt;&lt;STRONG style="border: none windowtext 1.0pt; padding: 0cm; color: #3d9ce7; font-size: 9.0pt;"&gt;MPC5744P_STCU2_BIST_v0_3.pdf&lt;/STRONG&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;) and example&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&lt;A _jive_internal="true" data-containerid="11363" data-containertype="14" data-content-finding="Community" data-objectid="334422" data-objecttype="102" href="https://community.nxp.com/docs/DOC-334422"&gt;&lt;SPAN style="color: #3d9ce7; border: none windowtext 1.0pt; padding: 0cm;"&gt;Example MPC5744P BIST On-line GHS614&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt; would be required? Or is some simpler sequence possible to use for this purpose?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0cm; margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;BR, Peder&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 12:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790630#M11550</guid>
      <dc:creator>pederrogo</dc:creator>
      <dc:date>2018-08-16T12:42:20Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790631#M11551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Well, I have to again ask.&lt;/P&gt;&lt;P&gt;1. do you want to inject physical fault into BIST?&lt;/P&gt;&lt;P&gt;2. or you need fault in BIST for SW reaction testing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because if 2. is the case. Then you simply program into MISR different values from recommended ones, or shorten watchdog timeout so BIST wont have time to finish, or..... there are many ways how to fake the BIST results.&lt;/P&gt;&lt;P&gt;But if 1. is the case, then your only chance is to play with voltages: VDD_HV, flash, core, etc...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 08:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790631#M11551</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2018-08-17T08:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790632#M11552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is enough with 2. It should not be needed to inject a physical fault. But, how to actually accomplish 2? For example we can set&amp;nbsp;LB0_MISRELSW to another value than&amp;nbsp;0x6D73AE0D, But, that is not enough? An on-line BIST has to be initiated?&lt;/P&gt;&lt;P&gt;But, actually we would like to fake a fault detected by the off-line BIST as we don't plan to use the on-line BIST.&lt;/P&gt;&lt;P&gt;Peder&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 13:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790632#M11552</guid>
      <dc:creator>pederrogo</dc:creator>
      <dc:date>2018-08-17T13:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying the Built-in Self-Test (BIST) on the MPC5744P</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790633#M11553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;If you want to do it for offline BIST then you must modify MISR for offline BIST.&lt;/P&gt;&lt;P&gt;This can only be done via DCF records.&lt;/P&gt;&lt;P&gt;However you can also fake your SW and consider that 0 in ERR_STAT is fault state so you can test your reaction path this way.&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 13:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Verifying-the-Built-in-Self-Test-BIST-on-the-MPC5744P/m-p/790633#M11553</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2018-08-17T13:42:15Z</dc:date>
    </item>
  </channel>
</rss>