<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [mpc5777c] Can I initialize less than 64 bits in Ram memory ? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777859#M11303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it must be 64-bit write to completely define ECC code for data unit. Otherwise you will have ECC error on that place.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Feb 2018 18:52:34 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2018-02-27T18:52:34Z</dc:date>
    <item>
      <title>[mpc5777c] Can I initialize less than 64 bits in Ram memory ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777858#M11302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Expert&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I write at the below page, I found how to initialize 64 bits of Ram memory.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/986762?commentID=986762#comment-986762" title="https://community.nxp.com/message/986762?commentID=986762#comment-986762"&gt;https://community.nxp.com/message/986762?commentID=986762#comment-986762&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But my customer wants to initialize only 1 byte of Ram memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I know, it is impossible because the e_stmw is the only one instruction I can use to initialize the Ram.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to initialize only 1 byte of Ram memory ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Jaejyn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 09:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777858#M11302</guid>
      <dc:creator>jaejynshin</dc:creator>
      <dc:date>2018-02-27T09:40:51Z</dc:date>
    </item>
    <item>
      <title>Re: [mpc5777c] Can I initialize less than 64 bits in Ram memory ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777859#M11303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it must be 64-bit write to completely define ECC code for data unit. Otherwise you will have ECC error on that place.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 18:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777859#M11303</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-02-27T18:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: [mpc5777c] Can I initialize less than 64 bits in Ram memory ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777860#M11304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your quick answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know the reason what it must be 64 bit.&lt;/P&gt;&lt;P&gt;It is&amp;nbsp;due to the because manual in MPC5777CRM_rev6 ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20529i13074055035BD143/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20499i13CECE0B4B1C3E6E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Jaejyn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 01:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777860#M11304</guid>
      <dc:creator>jaejynshin</dc:creator>
      <dc:date>2018-02-28T01:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: [mpc5777c] Can I initialize less than 64 bits in Ram memory ?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777861#M11305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you have answered yourself. "Less than 64-bit write" consists of read-modify-write sequence. If you have uninitialized 64-bit data word, write to any smaller portion of this word performs read-modify-write, and the read will cause ECC error exception (IVOR1 - machine check).&lt;/P&gt;&lt;P&gt;Initialization must be done by 64-writes, there is no other option. ECC error free data then can be accesses by less than 64-bit accesses, of course.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 09:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/mpc5777c-Can-I-initialize-less-than-64-bits-in-Ram-memory/m-p/777861#M11305</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-02-28T09:03:56Z</dc:date>
    </item>
  </channel>
</rss>